Technical FAQs

Ask a Question

ISX Central graphs may not include all data points including some peaks or valleys.

Issue:

ISX Central graphs may not include all data points including some peaks or valleys.

Product Line:

InfraStruxure Central / Struxureware Data Center Expert.

Environment:

Any version

Cause:

When graphs are created in the InfraStruxure Central client Reports perspective, the number of raw data points returned from the InfraStruxure Central server may be reduced.

Resolution:

Graphing numeric sensor data containing 10,000 data points and under: An algorithm retains significant outliers in the data set, for example, a spike or a drop in temperature or voltage.

Graphing numeric sensor data containing over 10,000 data points, or state sensor data: An algorithm reduces the data points to reach the maximum number of points to graph while retaining the overall shape of the data. The number of sensors, the time range of the report, and the total number of data points returned from the server is considered. Minimum or maximum data points for isolated spikes or drops may be eliminated.
 
Was this helpful?
What can we do to improve the information ?