Technical FAQs

Ask a Question

Using the Male to Male BNC Adapter Included in a Day/Night CCTV Camera (NBAC0224)

Issue:

Using the Male to Male BNC Adapter Included in a Day/Night CCTV Camera (NBAC0224)

Product Line:

NetBotz

Environment:

NetBotz NBAC0224

Cause:

Physical configuration options.

Resolution:

The NetBotz Day/Night CCTV Camera has a BNC female output.

The NetBotz CCTV Pod has BNC connection that looks like a male connector but it actually has a hole in the male connection so it will accept the male-male adaptor included with a Day/Night CCTV Camera.


Was this helpful?
What can we do to improve the information ?