Technical FAQs

Ask a Question

How can I extend the cable length of a Symmetra LX or Symmetra RM XR battery frame?


Issue

How can I extend the cable length of a Symmetra LX or Symmetra RM XR battery frame?


Product Line

Symmetra LX


Environment

All serial ranges


Cause

The need may arise for there to be space between the UPS mainframe and XR frames i.e. if they cannot be installed in the same rack or enclosure.


Resolution

There are two kits that would allow you to extend the length of a Symmetra RM or Symmetra LX extended run frame cable.

SYOPT4: 4ft (1.2m) Extension Cable

SYAOPT5: 15ft (4.6m) Extension Cable


Please Note: These cables are NOT compatible with the legacy SYXR4 and SYXR12 Extended Run cabinets designed for use with Symmetra Power Array.

 

Was this helpful?
What can we do to improve the information ?