Technical FAQs

Ask a Question

The Matrix-UPS battery communication cable has been misplaced, what can I do?


Issue

Replacement battery communication cable for Matrix battery pack is needed.


Product Line

Matrix-UPS


Environment

All serial numbers


Cause

The cable is damaged or has been misplaced.


Resolution

The cable that provides battery communication is a standard RJ9 2 line 4 wire head set cable.  This is available at any phone accessory supplier.


Was this helpful?
What can we do to improve the information ?