Technical FAQs

Ask a Question

Material Safety Data Sheets (MSDS) for Symmetra PX2 and PX 250-500kw UPS

MSDS information for various battery manufacturers utilized in Symmetra PX2 and PX 250/500 UPS systems

Symmetra PX2, Symmetra 250-500

All models/ All serial numbers

The rules regarding MSDSs changed in 2016 and it’s no longer sufficient just to post a link to the battery MSDS that we use.  When the rules changed, we began authoring Safety Data Sheets (new name for MSDSs) that would meet the new regulations.  These newly authored Safety Data Sheets (SDS) are located at the following web page.

You’ll note changes –
Safety Data Sheets are region specific.  There is a NAM format and an EU format.  

The intent is to direct all customers to this location when they have SDS or MSDS questions.


Was this helpful?
What can we do to improve the information ?