Technical FAQs

Ask a Question

Video: Manually Operating the APC Symmetra™ PX 250/500 UPS Battery Breaker

Issue:
How to Manually operate the Battery Breaker on a Symmetra 250-500kW UPS
 
Product line:
Symmetra PX 250-500
 
Environment:
All Product models, all serial numbers
 
Cause:
In the event the battery breaker does not automatically close during the startup of the ups you may need to manually close it.

Resolution: 
When the Breaker is Off (open) the indicator on the right will be green.
Push the lever on the left down and ‘Pump’ it until the indicator turns ‘Yellow’ Indicating Charged.
Once Charged, press the green button to turn the breaker on. The indicator will turn Red indicating the breaker is on.
 
To turn off, just press the off button.

The following video demonstrates this procedure:

Was this helpful?
What can we do to improve the information ?