Technical FAQs

Ask a Question

Symmetra PX 250/500; AP9635; Flood of RTC Time adjusted values in the logs

Issue:
Flood of RTC Time adjusted values in the logs
 
Product line:
Symmetra PX 250/500 with AP9635
 
Environment:
All Product models, all serial numbers
 
Cause:
When 2 Network Management Card (NMC) are installed in the UPS and set to NTP (Network Time Protocol), they will fight for control of the time to the display and continually send info alerts on RTC Time Adjusted.  In the chart below you will notice in column 5 there are two different numbers 2 & 4, which would indicate that there is 2 NMC in the UPS one in position #2 and the other in position #4.  This is the indicators that 2 NMC are fighting to provide time through NTP
 
46934 Info IM internal memory for storing configuration settings is OK IO enclosure level 3 pos E    02-26-2015 17:12:53 006
46933 Info RTC Time adjusted value Parallel UPS 1  2   02-26-2015 17:12:53 000
46932 Info RTC Time old value   2   02-28-2015 17:12:57 446
46931 Info IM internal memory for storing configuration settings is OK IO enclosure level 3 pos E    02-28-2015 17:12:49 006
46930 Info RTC Time adjusted value Parallel UPS 1  4   02-28-2015 17:12:49 000
46929 Info RTC Time old value   4   02-26-2015 17:12:44 548
 
Resolution:
Set only one of the NMC to NTP
 

 
Was this helpful?
What can we do to improve the information ?