Technical FAQs
Technical FAQs
Alert Action | Results | Prerequisites |
---|---|---|
Send Email | Sends an email via SMTP to one or more target recipients | none |
Send Short Message Email | Sends a custom formatted email via SMTP to one or more target recipients | none |
Send SMS Message | Sends an SMS text message via GSM service provider | GPRS / GSM Wireless Adapter |
Send SNMP V1 Trap | Sends an SNMP version 1 trap to configured targets | none |
Send HTTP POST | Sends standard (all) alert information formatted in XML to a web server in the form of an HTTP POST | Properly configured web server and application code |
Send Custom HTTP Get | Sends customized alert information to a web server in the form of an HTTP GET | Properly configured web server and application code |
Send Data to FTP Server | Sends standard alert data formatted in XML to an FTP server. | Properly configured FTP server |
Send Custom Text File to FTP Server | Sends custom alert text file to an FTP server | Properly configured FTP server |
Set Switch Output State | Sets the state of an device switch | Supported output device such as Output Relay Pod, Power Control Pod or third party intelligent power strip |
Activate Button State | Activates a push button defined on an output device | Supported output device such as Output Relay Pod, Power Control Pod or third party intelligent power strip |
Play Audio Alert | Plays or speaks the text of the alert | NetBotz 500, Camera Pod 120 and attached external, power speakers |
Call Web Services Alert Receiver | Sends customer alert information via the Web Services API to a remote system | Properly configured web server running custom application code integrated with the NetBotz Web Services API |