Print View   印刷用ページ  |   Email Press Release   電子メール  |   Facebook Twitter Digg DelIcioUs


APC Announces New InRow RD Modular Cooling System Ideal for Server Room and Data Centre Deployment


Row-Based Direct Expansion Cooling Solution Ensures Proper Airflow Paths and Increases Energy Efficiency

SYDNEY- AUSTRALIA: – March 26, 2009 – APC by Schneider Electric, a global leader in integrated critical power and cooling services, today announced the APC InRow RD, its new 300mm row-based, direct expansion cooling solution for network closets, server rooms and data centres. Key features of the APC InRow RD include real time capacity monitoring and easy operation, as well as variable speed fans that reduce energy consumption during off-peak hours. In addition, the modular design provides scalable solutions to add cooling as demand increases, up to 10kW.

With consolidation, power over Ethernet and virtualization making traditional server rooms increasingly complex, a cooling issue can be a contributing factor to ongoing power problems. Designed for installation within the row of racks, the APC InRow RD captures hot exhaust air directly from the aisle and distributes cool air through the front of the unit, which ensures temperatures are held at setpoint conditions.

“Larger and more complex server rooms are invariably running into one or more serious power problems as they expand,” noted Gordon Makryllos, Country General Manager for APC, Australia and New Zealand  “The goal of APC’s products is to grant unprecedented visibility into the inner workings of the server room, enabling users to monitor equipment effectively, identify issues before they become significant problems and truly manage the environment.

“With this goal in mind, the new APC InRow RD was designed to address server room issues in a unique, modular fashion that can help prevent downtime whether it is used by a small business or enterprise branch office,” Makryllos continued. “Placing the APC InRow RD unit in the row of racks moves the source of cooling closer to the heat load. This prevents the air from mixing and provides a predictable cooling architecture, allowing for tremendous flexibility and savings on installation as well as operation.”
The APC InRow RD is controlled by a microprocessor that provides a high level of functionality over the unit’s controls through a four line alphanumeric display and enables centralized management via the APC InfraStruXure Central.

The APC InRow RD Air Cooled and Fluid Cooled 300mm models are a global offering currently available Australia & New Zealand. To learn more about this and other APC cooling solutions for high-density applications, please visit www.apc.com or contact APC Australia 1800 652 725 or New Zealand 0800 333 373.


About APC by Schneider Electric

APC by Schneider Electric, a global leader in critical power and cooling services, provides industry leading product, software and systems for home, office, data center and factory floor applications.  Backed by the strength, experience, and wide network of Schneider Electric’s Critical Power & Cooling Services, APC delivers well planned, flawlessly installed and maintained solutions throughout their lifecycle.  Through its unparalleled commitment to innovation, APC delivers pioneering, energy efficient solutions for critical technology and industrial applications.  In 2007, Schneider Electric acquired APC and combined it with MGE UPS Systems to form Schneider Electric’s Critical Power & Cooling Services Business Unit, which recorded 2008 revenue of €2,6 billion (including APC-MGE sales of $3.7 billion) and employed 12,000 people worldwide.  APC solutions include uninterruptible power supplies (UPS), precision cooling units, racks, physical security and design and management software, including APC's InfraStruXure® architecture, the industry’s most comprehensive integrated power, cooling, and management solution.  Schneider Electric, with 114,000 employees and operations in 100 countries, achieved sales of €18,3 billion in 2008.  For more information on APC, please visit www.apc.com.  All trademarks are the property of their owners.

#   #   #


For more information contact:

n2n Communications
Contact: Alex Tudge
Phone: +61 2 9213 2320
Fax: +61 2 9212 0366
atudge@n2n.com.au

APC by Schneider Electric
Contact: Andra Mednis, Marketing Director
Phone: +61 2 8923 9331