View Services for Solutions

Implement a Data Center Consolidation / Virtualization Project

Increase availability with physical infrastructure that automatically and dynamically responds to migrating virtual loads
Reduce energy by an additional 30% beyond IT energy savings
Rapidly deploy power & cooling distribution to support high density zones which result from consolidation

How Schneider Electric can help
Infrastructure Management software to enable the automatic movement of VMs to healthy host machines based on the availability of power and cooling resources
Modular, scalable power & cooling solutions that enable right-sizing to match consolidated or growing IT loads
Close-coupled, row-based cooling solutions with variable speed fans that adjust to migrating IT loads in real time
Containment solutions such as the hot aisle containment system to meet high density zone requirements
Real-time physical infrastructure planning and management tools to maintain predictable operation even after moves, adds, and changes

Next Steps