Technical FAQs

Ask a Question

What are the condenser pressure drop and temperature limitations on the ACSC?

Issue:
What are the condenser pressure drop and temperature limitations?
 
Product line:
ACSC100, ACSC101
 
Environment:
InRow Cooling
 
Cause:
 
Resolution:
It is recommended that you have no more than 0.25” (65 Pa) of additional external pressure drop. The condenser should see inlet temperatures of 32-105 F (0-40 C), 70-86 (21-30 C) in ideal conditions. See Application Note #109 for further details.
Was this helpful?
What can we do to improve the information ?