Technical FAQs

Ask a Question

Network Air FM Field Fix Solution Chemical Propeties and MSDS Sheet


                                                                                                                                                           

Issue:  
Network Air FM Field Fix Solution Chemical Propeties and MSDS Sheet 

Product line:
ACFM, Network Air FM, IR40 

Environment:  
All Serial Numbers 

Cause:  
Install, Technical Information

Resolution:    

Coil Wetting Aid Field Fix 3 

Field Fix 3 is a liquid product formulated to promote a hydrophylic fin surface in aluminum evaporator coils. This product is a blend of wetting agents and surface active materials that penetrates residual rolling oils and fin lubricants and promotes the formation of aluminum hydrate on the fin surface. The hydrate formation provides permanent improved fin wettability and system performance. The product is used as received, no dilution is necessary. Simply apply product via spray, dip or fog to the coil surface. Allow product to dry in coil before putting into use. Residual product will be rinsed away with condensate water and leave a hydrophilic fin surface.To obtain samples or application information, please contact one of our customer service representatives.
Custom Formulating and Blending, Inc.
17716 Commerce Drive
Bristol, IN 46507
Phone (574) 848-5288 Fax (574) 848-5963 

Was this helpful?
What can we do to improve the information ?