Containment and Air Distribution

Managing airflow for rows, racks and hot spots


 
The EcoAisle is an intelligent thermal containment solution designed to increase cooling system efficiency while protecting critical IT equipment and personnel. The Active Flow Control (AFC) availble in the EcoAisle provides the intelligence to communicate to the cooling system in order to right size the cooling airflow to match the load of the IT equipment providing a reduction in fan energy over conventional cooling systems. The Eco Aisle system adapts to varying rack heights, aisle widths, and rack depths to support either hot or cold aisle containment. The Air Return System of the EcoAisle provides a centralized hot air return path for room based CRAC/CRAH units or external air handling systems. The optional UL723s listed Fire Safe System uses temperature sensors to drop ceiling panels in the event of a fire. The Fire Safe System can also be used in conjunction with a field supplied smoke detector to activate in the event smoke is detected with the aisle. EcoAisle provides a safe and efficient environment for IT equipment and personnell incorporating additional features for high efficiency LED lighting with motion detection. EcoAisle can be deployed in zones or modules to gain the benefit at either the rack or row level.
Read More
These rack-based cooling products are specifically integrated in or on individual rack enclosures to solve inadequate air distribution problems. Rack Air Distribution systems work with existing cooling products to either provide cool air to or remove heat from the rack enclosure. These hot spot problem solvers ensure uniform inlet temperatures to the IT equipment.
Read More
Wiring closet heat loads are rising due to deployment of technologies such as VoIP and Power over Ethernet. Many closets where these technologies are being deployed are not designed with adequate air distribution. The Wiring Closet Ventilation Unit is a rapidly deployable wall or ceiling mounted air distribution and heat removal system designed specifically for the wiring closet environment. By exhausting hot air from the closet to an adjacent space, it allows conditioned air (entering through the Air Intake Grill) to cool the load. This budget conscious unit is an excellent alternative to more expensive air-conditioning systems, providing reliable heat removal with the capability to lower closet temperatures by up to 40ºF (22ºC). If plugged into a UPS, it can also be used as a back-up heat removal system to an already existing air-conditioning unit to maximize system availability in the event of a power failure. Dual fans increase availability while LED status indicators and dry contact outputs enhance the unit’s manageability. Selectable fan speeds allow the user to choose between maximum performances.
Read More