Technical FAQs

Ask a Question

Video: How to take Silcon UPS out of Maintenance Bypass (MBP)

Issue:
How to take Silcon UPS out of Maintenance Bypass (MBP)
 
Product line:
Silcon
 
Environment:
All Product models, all serial numbers
 
Cause:
This video provides a step by step instruction on how to operate the Silcon UPS from Maintenance Bypass mode, to allow the end-user to transfer load back onto the UPS, without interruption to their load.
 
Resolution:
Display will say Bypass Operation
The Green LED (H002) above Q002 will be illuminated; you can now turn Q002 to ON (Center)
The Green LED (H003) above Q003 on the bypass panel will be illuminated; you can now turn Q003 to off (Right)
Press # key
Use the arrow keys to scroll to Bypass Operation: Yes
Press the C key to change to Bypass Operation: No
Press # to store – Display will flash the message “Data Stored”
UPS will go to Normal operation
The Green LED (H002) above Q002 on the bypass panel will go off
 
 
Was this helpful?
What can we do to improve the information ?