Technical FAQs

Ask a Question

What are the Minimum and Maximum mounting depths for Smart-UPS rails?


Issue:

What are the Minimum and Maximum mounting depths for Smart-UPS rack mount rails?

Product Line:

Smart-UPS

Environment:

All rack mounted models, All Serial Numbers

Cause:

Smart-UPS Rackmount UPS units (typically designated with "RM" in the part number) include a system of rails and brackets to mount the unit in a typical IT rack enclosure. The rails are adjustable to allow for a range of different sized racks. For specifics of how to mount your unit, please refer to the installation documentation included with your UPS.

Resolution:

For all Smart-UPS products 10Kva or less:
The minimum depth for the rails is 21.75" and the maximum depth is 36".
NOTE: If your Smart-UPS is equipped with cleats (metal pieces attached to the sides of the Smart-UPS chassis that slide into the rails) the minimum depth is 29"".

For Smart-UPS products over than 10Kva:
The minimum depth for the rails is 27.5" and the maximum depth is 33".


 

If you are using your APC rail kit to mount non-APC equipment your experience may vary. 
Please note that some networking specific or custom enclosures may need to be adjusted to accommodate the depth of the rails.

Was this helpful?
What can we do to improve the information ?