Schneider Electric’s Next-Gen Cooling Solution Now Available across Gulf region

Schneider Electric’s Next-Gen Cooling Solution Now Available across Gulf region

  • InRow DX cuts 50 percent more energy than first generation technology
  • Delivers energy efficiency for high capacity loads
  • New user interface and enhanced controls lower energy costs

Dubai (UAE), July 24, 2016Schneider Electric, a global specialist in energy management and automation, today introduced the second generation of the InRow DX (direct expansion) 600mm as the latest addition to the InRow product line, expanding Schneider Electric’s vast cooling portfolio to meet the evolving cooling needs of an ever-changing data center environment. Given the growing demand for density cooling and temperature management in data center, the InRow DX has been designed to lower energy costs and features enhanced controls and a new user interface.

Datacenters are experiencing exponential growth in the region. At the same time, there is a heavy focus on curtailing energy costs and mitigating the carbon footprint towards sustainability. IT equipment and sensitive technology which utilizes electricity also emits heat as a waste product. Advanced cooling solutions have thus become critical to the smooth functioning of a datacenter, and to the maintenance of hardware carrying mission-critical enterprise data. In fact, a 2015 Research and Markets study states that the datacenter cooling market in the GCC will grow at a CAGR of 23.37 percent over the period 2014 to 2019.

With the second generation InRow DX release, enterprises can significantly improve cooling efficiency by reducing power consumption while increasing capacity. Capable of high-density cooling up to 42kW with a 4000 SCFM max airflow in a small 600mm-wide footprint, this solution provides the highest partial-load energy savings in the industry, cutting energy consumption 50 percent more than the first generation technology. This is enabled by the use of new brushless variable speed scroll compressors and EC fans, making the new InRow DX 600mm the most efficient system of its class.

Pay as you Grow
The InRow DX design closely couples cooling with the IT heat load, preventing hot air recirculation, while improving cooling predictability and allowing for a pay as you grow environment. Available in self-contained, fluid-cooled, and air-cooled configurations with or without humidity control, these products meet the diverse requirements for closet, server room, and data center cooling.

Active Flow Control
The addition of Active Flow Control, which measures air pressure inside the containment system and automatically adjusts fan speed to match the exact airflow of the IT equipment, increases precision and efficiency. With an improved user-friendly design, the InRow DX also features an intuitive 4.3-inch color touch screen display and network card, to provide fast, easy access to data and increased visibility into cooling system performance.

“Data center managers face numerous obstacles on the path towards efficiency, including growing performance needs resulting in higher density systems, tightening energy regulations and pressure to reduce OpEx,” said Anne-Marie Gignac, VP, Cooling Business, Schneider Electric. “The latest generation of InRow direct expansion cooling puts efficiency and cost savings at the forefront for users, delivering the greatest partial-load energy savings available in a small but powerful system.”

The InRow DX 600mm is now available for purchase in the Gulf region through Schneider Electric’s distributors and resellers. For more information on Schneider Electric’s InRow product line, please visit the Schneider Electric InRow Direct Expansion web page.

Related resources: