Technical FAQs

Ask a Question

Can I run cables over the SC? If so, how many?


Issue:  
Can I run cables over the SC? If so, how many?

Product line:
ACSC1XX

Environment:  
All Serial Numbers

Cause:  
FAQ

Resolution:
 
Yes, there is a cable support bridge trough available as an accessory (ACAC10021). You will need (2) per SC unit to carry
both data and power cables across the unit. Approximately 80 CAT5 cables or 8 power whips fit into a trough.
 
 
 
Was this helpful?
What can we do to improve the information ?