Technical FAQs

Ask a Question

How to troubleshoot compressor issues


                                                                                                                                                           

Issue:
How to troubleshoot compressor issues. 

Product line: 
All Compressor Equipped Cooling Units. 

Environment: 
All Serial Numbers.     

Cause:  
Troubleshooting  

Resolution:    

Problem

Possible Causes

Possible Corrective Steps

Compressor will not run

1) Main Switch Open

1) Close switch

 

2) Fuse Blown

2) Check electrical circuits and motor winding for shorts to ground.  Investigate for possible overloading.  Replace fuse after fault is corrected.

 

3) Thermal Overloads tripped

3) Overloads are automatically reset.  Check unit closely when unit come back on line

 

4) Defective contactor/coil

4) Repair/replace

 

5) System shut down by safety devices

5) Determine type and ause of shutdown and correct it before resetting safety switch

 

6) No Cooling required

6) None.  Wait until calls for cooling.

 

7) LL solenoid will not open

7) Repair/replace LL coil

 

8) Motor electrical trouble

8) Check motor for open winding, short circuits, or burnout

 

9) Loose wiring

9) Check all wire junctions.  Tighten all terminal screws.

 

10) Trouble in starting switch or control circuit

10)  Close switch manually to test
power supply. If OK check control
circuit including temperature and
pressure controls

 

11)  Seized compressor

11) Repair/replace

     

Compressor noisy/vibrating

1) Check for liquid or slugging

1) Check expansion valve(s); check oil levels

 

2) Improper piping supports

2) Relocated, add/remove hangers

 

3) Worn compressor

3) Repair/replace

     

High Discharge Pressure

1)  Air or non-condensable gas in
system

1) Remove non-condensables

 

2) Insufficient cooling of air-cooled condenser

2)  Check fan operation, cleanliness of
condenser, and for adequate source of air flow

 

3) System overcharge / Too much liquid in receiver

3) remove excess

 

4) Discharge service valve partially closed

4) Open valve

 

5) Fan not running

5) Check electrical circuit

 

6) Head pressure control setting

6) Adjust

 

7) Dirty Condenser coil

7) clean

water/glycol only

8) Insuffiecient water flow/failed pump

8) Increase gpm/repair/replace

water/glycol only

9) Inlet water warm

9) Adjust/fix/repair

water/glycol only

10) Fouled HX

10) Clean/flush, replace

water/glycol only

11) Actuator/3-way valve failed

11) Repair/replace

     

Low Discharge pressure

1) Faulty condenser temperature regulation.

1) check condenser control operation

 

2) Insufficient refrigerant in the system

2) check for leaks, repair, add charge

 

3)Low suction pressure

3) see corrective steps for low suction pressure.

 

4) Variable head pressure valve

4) check valve setting

 

5) Hot gas by pass operation

5) check operation

     

High Suction pressure

1) excessive load

1) Reduce load or add additional equipment

 

2) Expanve valve overfeeding

2) Check TEV bulb, regulate SH.

     

Low Suction Pressure

1) Insufficient refrigerant in system

1) Check for refrigerant storage

 

2) Expansion valve power element dead, malfunctioning, or weak.

2) Replace expansion valve power element

 

3) Low refrigerant charge

3) Locate and repair leaks. Charge refrigerant

 

4) Improper adjustment of expansion valve

4) Adjust valve to give more flo

 

5) Condensing temperature too low

5) Check meas for regulating condensing temperature

 

6) Clogged suction line

6) Clean

 

7) Clogged LL filter drier

7) Remove/ replace

     

Compressor Short Cycles

1)  Low refrigerant charge

1) Leak check and add if necessary

 

2) No load

2) To prevent short cycling, if objectionable, need to add false load

 

3) Unit is too large for load

3) Reduce compressor speed; Install false load system

     

Compressor runs continuously

1) Shortage of refrigerant.

1) Repair leak and recharge system.

 

2) Leaking discharge valves.

2) Replace discharge valves

     

 

 

 

 

 

In
Was this helpful?
What can we do to improve the information ?