Technical FAQs

Ask a Question

Can I use the Camera pod 160 with Netbotz Version 2 appliances (Netbotz 500 and Netbotz 420 models)

Issue:

Will the NBPD0160 camera pod work with the older version 2 NetBotz appliances?

Product Line:

NetBotz

Environment:

Netbotz version 2

Cause:

NetBotz camera pod NBPD0121 is no longer manufactured.

Resolution:

No, a NBPD0160 NetBotz camera pod must be used with a version 3 NetBotz appliance. However, an version 2 NetBotz camera pod (NBPD0121) can be used with a version 3 NetBotz appliance.
 
Was this helpful?
What can we do to improve the information ?