RWANDA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
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
Data Center Assessment Services
Install
Installation Services
Operate
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
RWANDA - Choose Country or Region
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
How quiet (or noisy) is the NetShelter CX when only the fans are running, with no equipment installed?
Issue:
Customer wants to know how quiet the cabinet is with nothing installed, just the fans running.
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
Noise reduction in the office is important.
Resolution:
Noise of AR4018A / AR4018IA:
40.5 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet
Noise of AR4024A / AR4024IA:
43.0 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet
Noise of AR4038A / AR4838IA:
43.5 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet