Technical FAQs

Ask a Question

Can a 63.75" tall PDU be installed into a 38U NetShelter CX cabinet?

The 63.75" tall PDU does not fit onto the accessory rail. Will it fit anywhere else inside the cabinet? 

Product Line: 
NetShelter CX 

AR4038A, AR4038IA

A customer wants to install one of the 63.75" tall PDUs into a 38U NetShelter CX cabinet. 

Yes, the 63.75" tall PDUs can attach to the rear mounting rail. Please see the attached file for mounting instructions. 
Was this helpful?
What can we do to improve the information ?