Technical FAQs

Ask a Question

Do the NetShelter CX cabinets have dedicated ground points?

The customer is looking for a ground point on the cabinet. 

Product Line:
NetShelter CX

All versions and serial ranges.

The customer wants to bond the equipment or various parts of the cabinet to a ground. 

The NetShelter CX cabinets no not currently have a dedicated ground point. 
The CX cabinet is intended to be used with certified equipment that provides a proper enclosure to guard against electrical hazards.  Proper ground for these types of equipment is made through the attachment of the plug/cord and provided this ground path exists to the supply PDU, there is no need for external grounding of the rack. 
Was this helpful?
What can we do to improve the information ?