Technical FAQs

Ask a Question

What are the dimensions of the door handle cutout on the NetShelter SX?

Issue:
We are being asked to provide the dimensions of the door handle cutout.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Customers wishing to use a 3rd party door handle need to know the size of the door handle cutout.

Resolution:
The dimensions of the NetShelter SX door handle cutout are: (H) 150 mm x (W) 25.5 mm.  (6" x 1")
Was this helpful?
What can we do to improve the information ?