Technical FAQs

Ask a Question

Video: How to place Galaxy VM UPS into Maintenance Bypass

Issue:
How to place Galaxy VM UPS into Maintenance Bypass
 
Product line:
Galaxy VM
 
Environment:
All Product models, all serial numbers
 
Cause:
The UPS must be transitioned into maintenance bypass mode for certain types of service or other maintenance to the system.
 
Resolution:
Push the Home screen Icon
Push CONTROL, default password 1234
Select SHUTDOWN WIZARD
Select Shutdown ending in Maintenance Bypass, now follow the on screen instructions

This video provides a step by step instruction on how to transition the Galaxy VM UPS into Maintenance Bypass mode, allowing the end-user to power down the UPS without interruption to their load.
 

 
Also see article FA243122 to take unit out of Maintenance Bypass
Was this helpful?
What can we do to improve the information ?