Technical FAQs

Ask a Question

Install error message "A test command parameter is not valid " is shown when the installation is initiated on HP-UX

Issue:
When installing PowerChute Network Shutdown on HP-UX an error message appears "A test command parameter is not valid".

Product:
PowerChute Network Shutdown versions 3.0.1 and 3.1

Environment:
HP-UX 11i v3

Cause:
Invalid parameter

Solution:
Ignore the error. The installation will proceed.
Was this helpful?
What can we do to improve the information ?