Technical FAQs

Ask a Question

Do all NetShelter SX cabinets ship with the same key?

Issue:
A customer needs to know if all NetShelter cabinets ship with the same key.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Having a single key allows ease and simplicity for customers who own multiple cabinets. Or, someone may want unique keys on some cabinets.

Resolution:

Yes, all NetShelter SX cabinets ship with the same key for the front door, rear doors and side panels.
If you would like information on unique locks for NetShelter SX cabinets please see Knowledge Base document FA158606.
If you need replacement keys for a NetShelter cabinet please see Knowledge Base document FA158623.

Was this helpful?
What can we do to improve the information ?