Technical FAQs

Ask a Question

Video: How to reset all run hours on InRow Cooling systems.

Issue:
How to reset all run hours on InRow Cooling units.

Product line:
All InRow Products

Environment: 
All Serial Numbers

Cause:
Repair, Maintenance 

Resolution:



Run hours
The cooling unit records the number of hours each of its components has operated. When a component is replaced, use the Reset Run Hours option to reset the run hours for the displayed component to zero.
 
Path: Main > View Run Hours
• Air Filter
– Reset Run Hours
 
• Fans
– Fan Number
• Reset Run Hours
 
• Compressor
– Reset Run Hours
 
• Condensate Pump
– Reset Run Hours
 
• Fan Power Supplies
– Reset Run Hours
 
 
Was this helpful?
What can we do to improve the information ?