Technical FAQs

Ask a Question

Are the NetShelter CX and CX Mini delivered fully assembled?

Issue:
Need to know if the NetShelter CX and Mini arrive assembled.

Product Line:
NetShelter CX
 
Environment:
All versions and serial ranges.
 
Cause:
Customers may ask if assembly is required.
 
Resolution:
The NetShelter CX Mini arrives on its castors with the brush strip attached to the underside, on a pallet, and the keys inside.
The NetShelter CX arrives on a pallet with ramps supplied. The PDU power cord, leveling feet, keys and documentation are packed separately inside the cabinet.
 
Was this helpful?
What can we do to improve the information ?