Technical FAQs

Ask a Question

Large device discoveries in StruxureWare may affect performance.

Issue:

Discovering large numbers of nodes in StruxureWare Central or StruxureWare Data Center Expert can result in performance issues, sometimes requiring a system reboot.

Product Line:

StruxureWare Data Center Expert
StruxureWare Central
InfraStruxure Central


Environment:

All current versions

Cause:

Discoveries send larger amounts of data requests than normal scans. In many cases, other files such as configuration files and DDF files are also transferred during discovery

Resolution:

For best results, it is recommended that a large discovery job, for example 2000 SNMP devices, be run as several smaller discoveries.
 
Was this helpful?
What can we do to improve the information ?