Technical FAQs

Ask a Question

Export as AVI option in ISX Central not available for Pelco cameras.

Issue:
Export as AVI option in ISX Central not available for Pelco cameras

Product Line:
NetBotz
Pelco cameras

Environment:
Netbotz / Pelco camera integration

Cause:
Due to differences between ISX Central's image options and Pelco camera image options, clips exported using the AVI file type were exporting improperly.

Resolution:
This option may be fixed in a future revision but in ISX Central 5.1, the AVI export option has been removed for Pelco cameras.

Was this helpful?
What can we do to improve the information ?