Technical FAQs

Ask a Question

GPS Receiver Support for the NetBotz 500

Issue:

GPS Receiver Support for the NetBotz 500

Product Line:

NetBotz

Environment:

Version 2 NetBotz 500

Cause:

Supported configurations..

Resolution:

The NetBotz 500 supports the attachment of a GPS (global positioning system) receiver.
  • The NetBotz 500 reports GPS readings such as latitude, longitude, altitude, heading, velocity, and status as monitorable sensors
  • Current latitude and longitude readings can be attached to all alerts
  • Connects to WB500 USB port using USB-to-RS232 serial converter cable
  • Support for two NMEA-compliant GPS receivers:
    1. Garmin GPS35 USB
    2. Laipac G10-USB
Was this helpful?
What can we do to improve the information ?