Technical FAQs

Ask a Question

Video: How do I configure DNS on v3 NetBotz Appliances?

Issue:
Process for configuring DNS on v3 NetBotz Appliances.

Product Line:
NetBotz version 3

Environment:
NetBotz Model: 355, 455, 450, 550, or 570.

Resolution:



1) Log into your NetBotz Appliance as an administrator using the Advanced View application.

2) Select the Configuration Tab and then under Appliance Settings select DNS.


Configuring DNS Settings

1) Select the DNS pane (tab).

2) Enter the DNS domain.

3) Enter the DNS Servers that you would like to use (up to 3).

4) Click OK.


Configuring Dynamic DNS Settings

1) Select the Dynamic DNS pane (tab).

2) Check the box to Enable Dynamic DNS.

3) Fill in the required information for configuring Dynamic DNS.

4) Click OK.
Was this helpful?
What can we do to improve the information ?