Technical FAQs

Ask a Question

Video: How to check the model and serial number of an ACSC100

Issue:
How to check the model and serial number of an ACSC100
 
Product line:
ACSC100
 
Environment:
All serial numbers
 
Cause:
To help tech support identify the unit and its warranty status
 
Resolution:

 

Press the < ESC> button until you get to the “ON/STANDBY” screen. Then use the down arrow to scroll though the display. When you get to the screen “ABOUT INROW” stop and make sure the arrow on the left side of the display is pointing at it and the hit the <ENTER/RETURN> button.
 
Now you have access to:
 
MODEL
 
SERIAL NUMBER
 
FIRMWARE
 
HARDWARE
 
MFG DATE
 
APP
 
AOS VERSION

 
 
Was this helpful?
What can we do to improve the information ?