Technical FAQs

Ask a Question

Information overwritten if two StruxureWare Data Center Expert servers use the same remote repository.

Issue:

Information overwritten if two StruxureWare Data Center Expert servers use the same remote repository

Product Line:

StruxureWare Central / Data Center Expert

Environment:

StruxureWare DCE / Central any version

Cause:

If you add a remote repository that is already been used by another DCEl server, the repository.id file is overwritten (which contains the Mac address of the server and mounted date). This may cause problems if multiple servers are using the same remote share.

Resolution:

Each StruxureWare system needs it's own unique repository/shared folder.
 
Was this helpful?
What can we do to improve the information ?