Technical FAQs

Ask a Question

Update Email Address used to login to NetBotz Customer Portal (NetBotz Registration)

Issue:

Update Email Address used to login to NetBotz Customer Portal (register.netbotz.com)

Product Line:

NetBotz

Environment:

NetBotz registration portal

Cause:

Customer information.

Resolution:

NetBotz Customer Portal (NetBotz Registration Site) allows users to register products, activate extended warranty, view extended warranty status and license keys associated with appliances or servers, submit an electronic Support incident (if the appliance that a customer has questions about is in standard warranty or extended warranty), and etc.

Customers can update their E-Mail addresses via the portal:

1. Login to the portal using the existing "User Nam"" (an E-Mail Address) and "Password"
2. In 'My Profile' button, update 'E-Mail' field with a desired email address
3. In 'Password' and 'Confirmed Password' field, type the existing or new password, if you also wish to change password at the same time

If no error is indicated, E-Mail address and/or Password should be updated, and users will be brought back to the home page of the portal.

If users logs out the current session or closes the browser, users will need to use updated E-Mail address and/or Password to login to NetBotz Customer Portal.

Please note that going forward, the registration page for NetBotz may change.
Was this helpful?
What can we do to improve the information ?