Technical FAQs

Ask a Question

NetBotz Central 2.x and InfraStruXure Central Support OpenLDAP and Active Directory

Issue:

NetBotz Central 2.x and InfraStruXure Central Support OpenLDAP and Active Directory

Product Line:

NetBotz Central 
InfraStruxure Central
StruxureWare Data Center Expert

Environment:

NetBotz Central version 2
InfraStruxure Central all versions 
StruxureWare Data Center Expert servers, all versions

Cause:

Alternative authentication options

Resolution:

NetBotz Central 2.x and InfraStruXure(ISX) Central support Active Directory or OpenLDAP integration for user profile management. The Active Directory and OpenLDAP integration allows NetBotz/ISX Central to utilize the power of centralized profile management and centralized user IDs and passwords. Users added using this manner do not inherit any rights from the LDAP or AD server, rights Within the ISXC or DCE server are assigned within the local server's user management section
Was this helpful?
What can we do to improve the information ?