Technical FAQs

Ask a Question

InRoom Clearing the communication bus

Oftentimes if an InRoom unit, or group of units, is experiencing communication faults or other erroneous alarms, clearing the I/O bus will quickly and easily resolve the issue.

This can be done by pressing the right arrow repeatedly until the entire screen is selected (all blacked out), and then pressing the OK button.  You will be prompted for the password at this point (the default password is either 0000 or 2718).  Enter the password to complete the process.
Was this helpful?
What can we do to improve the information ?