Technical FAQs

Ask a Question

Which PCMICA Cards are supported by the APC Console Port Server?

You can find a list of supported PCMCIA cards through the Console Port Server itself. To do so, log into the Console Port Server via Hyperterminal/Telnet/SSH. Once logged in, issue the following command:
 

cat /etc/pcmcia/SUPPORTED.CARDS.

A list of supported cards should be displayed. Alternatively, please see the attached file for supported devices. 

Was this helpful?
What can we do to improve the information ?