The Smart-UPS SC is an entry level UPS for low power network and point-of-sale (POS) equipment. Please refer to application note #147 when using with servers that have active power factor corrected (PFC) and/or redundant power supplies.
付属: ユーティリティCD, マニュアルCD, ラックマウント用取り付けブラケット, Smart UPSシグナリング用RS-232ケーブル, USBケーブル, ユーザマニュアル
| (4) IEC 320 C13 |
|
| (2) IEC Jumpers |
| IEC-320 C14 |