Technical FAQs

Ask a Question

Video: How to Clear Alarms on an InRow ACRD200 Cooling System

Issue:
How Clear Alarms on an ACRD200 Cooling Unit

Product line: 
InRow Cooling Products ACRD200

Environment:
All Serial Numbers

Cause:
Install, Configuration

Resolution:



First you need to access the Clear Alarms menu you can do this by hitting the <ESC> until visible
 
Then select ENTER
 
It will ask if you want to clear alarms select yes
 
You will be prompted for a Password
 
Use the default password of “apc”
 
If this does not work check with your Admin for the correct password
 
If password has been lost use the last eight digits of the serial number
 
Now select clear alarms again and again select yes and alarms will be cleared.
 
 
Was this helpful?
What can we do to improve the information ?