Can I use the ACSC1XX with Hot Aisle Containment System (HACS)?
Issue:
Can I use the ACSC1XX with Hot Aisle Containment System (HACS)?
Product line: A
ACSC1XX
Environment:
All Serial Numbers
Cause:
FAQ
Resolution:
No, the HACS ceiling tiles will interfere with the condenser duct tubes. Also in configurations were HACS is required it will make more sense to offer the InRow RC, RD, or RP units.
.