The Version 2 Appliances have more features however to adjust such as which camera and resolution. To change these options, simply change the following values:
nbOwlEnc_0_CAMERA
Change the 0 to a 0 1 2 or 3 to select the desired camera.
Change QVGA to one of the following to select the desired resolution.