|
You are here:
|
Product Category |
PowerChute Network Shutdown Standard 1 node with upgrade license
SSPCNSS1UJ Features
Event logging
Pinpoint the timing and sequence of events leading up to an incident with the event log.
E-mail notification
Network administrators can solve problems remotely before they impact availability.
Scheduled shutdown and reboot
Customize shut down and reboot of connected equipment and UPSs.
Run command file
Run command file on shutdown sequence as well as start-up sequence.
Operating System Shutdown
Prevents possible data corruption by performing graceful, unattended operating system shutdown in the event of an extended power outage.
Server shutdown of N+1 UPS
Supports up to three UPS units in a redundant configuration. All UPS units in a redundant configuration must be of the same model.
PowerChute Network Shutdown Features & Benefits
Protection
Operating System Shutdown
Prevents possible data corruption by performing graceful, unattended operating system shutdown in the event of an extended power outage.
Shutdown Confirmation
In extended outages, UPS proactively coordinates and confirms safe, complete shutdown of all systems before UPS turns off.
Run command file
Run command file on shutdown sequence as well as start-up sequence.
Sequenced shutdown and reboot
Customize shutdown and reboot sequence of connected servers and UPSs.
Secure communications
Secured web access via HTTPS, as the default, ensures that communication between the device and the client interfaces cannot be interpreted.
Availability
Event logging
Pinpoint the timing and sequence of events leading up to an incident with the event log.
Manageability
Network-based shutdown
Reduces cable clutter by eliminating the need to connect the UPS and protected servers via cables.
Browser Accessible
View the user interface with a browser. Provides quick access from anywhere on a secure network.
UPS Status Checking
Continuously checks UPS status to verify current condition.
Step-by-step configuration wizard
Speeds deployment by reducing installation and set-up time. Allows configuration changes even after initial set-up.
Text-based INI configuration file
Allows for flexibility in archiving configuration settings or copying configured settings from one Agent to another.
Compatibility
PowerChute Network Shutdown OS Compatibility
This software supports numerous operating systems and processors. For further information, please
click here.
Server shutdown of N+1 UPS
Supports up to three UPS units in a redundant configuration. All UPS units in a redundant configuration must be of the same model.
Parallel-UPS configuration support
Recognizes a Parallel-UPS configuration as a single UPS system in the case of actionable events (for UPS devices that are parallel-capable).
Product Distribution
japan
|
||||||||