SGM Auto-shutdown software; v3.6 for Windows 7; Vista and XP (Brazil only) Product Overview

Application Shutdown Utilities

SGM Auto-shutdown software; v3.6 for Windows 7; Vista and XP (Brazil only)
SFSGM36
DISCONTINUED : recommended replacement product SFSGM38
Email Technical Specifications Printer Friendly
Locate a Partner

Easily configurable utilities for network administators that enables PowerChute to provide safe shutdown of mission-critical applications on servers.


Application Shutdown Utilities Features & Benefits

Protection
Four shutdown types
PowerChute Shutdown Utility for Oracle gives database administrators the flexibility to choose any one of the four Oracle shutdown types to meet the availability needs of the application
Convenience
Configure multiple instances
All instances on the server that need to be shut down are configured during the same session. The utility prompts the DBA for the requisite information to shut down each instance.