Availability
|
|
Automatic internal bypass
|
Supplies utility power to the connected loads in the event of a UPS overload condition or fault. |
|
Scalable runtime
|
Allows additional run time to be quickly added as needed. |
|
Intelligent battery management
|
Maximizes battery performance, life, and reliability through intelligent, precision charging. |
|
Hot-swappable batteries
|
Ensures clean, uninterrupted power to protected equipment while batteries are being replaced |
|
Automatic restart of loads after UPS shutdown
|
Automatically starts up the connected equipment upon the return of utility power. |
|
Temperature-compensated battery charging
|
Prolongs battery life by regulating the charge voltage according to battery temperature. |
| |
Manageability
|
|
Network manageable
|
Provides remote management of the UPS over the network. |
|
InfraStruXure Manager Compatible
|
Enables centralized management via the APC InfraStruXure Manager. |
|
SmartSlot
|
Customize UPS capabilities with management cards. |
|
LED status indicators
|
Quickly understand unit and power status with visual indicators. |
|
Serial Connectivity
|
Provides management of the UPS via a serial port. |
| |
Adaptability
|
|
Plug-and-Play external batteries
|
Ensures clean, uninterrupted power to the loads when adding extra runtime to the UPS. |
|
Rack/Tower convertible
|
Protects the initial investment in the UPS when migrating from tower to rack-mount environment. |
|
Flash upgradeable firmware
|
Install maintenance releases of firmware remotely using FTP. |
| |
Serviceability
|
|
User-replaceable batteries
|
Increases availability by allowing a trained user to perform upgrades and replacements of the batteries reducing Mean Time to Repair (MTTR) |
|
Automatic self-test
|
Periodic battery self-test ensures early detection of a battery that needs to be replaced. |
|
Predicitive failure notification
|
Provides early-warning fault analysis ensuring proactive component replacement. |
|
Disconnected battery notification
|
Warns when a battery is not available to provide backup power. |
|
Audible alarms
|
Provides notification of changing utility power and UPS conditions |
| |
Protection
|
|
Frequency and voltage regulation
|
Gives higher application availability by correcting poor frequency and voltage conditions without using the battery. |
|
Power conditioning
|
Protects connected loads from surges, spikes, lightning, and other power disturbances. |
|
Input power factor correction
|
Minimizes installation costs by enabling the use of smaller generators and cabling. |
|
Generator compatible
|
Ensures clean, uninterrupted power to protected equipment when generator power is used. |
|
Cold-start capable
|
Provides temporary battery power when the utility power is out. |
|
Resettable circuit breaker
|
Easy recovery from overloads; no need to replace a fuse. |
|
Safety-agency approved
|
Ensures the product has been tested and approved to work safely with the connected service provider equipment and within the specified environment. |
| |