ATTENTION: For instructions on how to properly link to these white papers.click here
6 result(s) found.
Number
Title & Abstract
WP-48 v1
Comparing Availability of Various Rack Power Redundancy Configurations Transfer switches and dual-path power distribution to IT equipment are used to enhance the availability of computing systems. Statistical availability analysis techniques suggest large differences in availability are expected between the various methods commonly employed. This paper examines various electrical architectures for redundancy that are implemented in today’s mission-critical environments. The availability analyses of these various scenarios are then performed and the results are presented. The analysis identifies which approach provides the best overall performance, and how alternatives compare in performance and value.
WP-27 v3
Efficiency and Other Benefits of 208 Volt Over 120 Volt Input for IT Equipment Decisions made regarding the distribution of 208V or 120V power to IT equipment can significantly impact overall efficiency of the data center. This paper explores the voltage connection options of 208 volt (V) and 120V for servers in North America and considers the efficiency implications of these choices. This same discussion applies to the use of 200V vs. 100V in Japan.
WP-28 v1
Rack Powering Options for High Density in 230VAC Countries Alternatives for providing electrical power to high density racks in data centers and network rooms are explained and compared. Issues addressed include quantity of feeds, single-phase vs. three-phase, number and location of circuit breakers, overload, selection of connector types, selection of voltage, redundancy, and loss of redundancy. The need for the rack power system to adapt to changing requirements is identified and quantified. Guidelines are defined for rack power systems that can reliably deliver power to high density loads while adapting to changing needs.
WP-43 v3
Dynamic Power Variations in Data Centers and Network Rooms The power requirement required by data centers and network rooms varies on a minute by minute basis depending on the computational load. This magnitude of this variation has grown and continues to grow dramatically with the deployment of power management technologies in servers and communication equipment. This variation gives rise to new problems relating to availability and management.
WP-29 v6
Rack Powering Options for High Density Alternatives for providing electrical power to high density racks in Data Centers and Network Rooms are explained and compared. Issues addressed include quantity of feeds, single-phase vs. three-phase, number and location of circuit breakers, overload, selection of plug types, selection of voltage, redundancy, and loss of redundancy. The need for the rack power system to adapt to changing requirements is identified and quantified. Guidelines are defined for rack power systems that can reliably deliver power to high density loads while adapting to changing needs.
Instructions for linking white paper content to your site
Since these white papers are often revised, to ensure your readers are receiving the most up-to-date content, it is important to use the following URL format when linking to these white papers:
http://www.apc.com/whitepaper/?wp=xxx
where "xxx" should be replaced with the number of the white paper being linked to.
Alternatively, the entire Schneider Electric data center white paper library can be linked to using the following url:
http://whitepapers.apc.com