ATTENTION: For instructions on how to properly link to these white papers.click here
3 result(s) found.
Number
Title & Abstract
WP-68 v1
Cooling Strategies for IT Wiring Closets and Small Rooms Cooling for IT wiring closets is rarely planned and typically only implemented after failures or overheating occur. Historically, no clear standard exists for specifying sufficient cooling to achieve predictable behavior within wiring closets. An appropriate specification for cooling IT wiring closets should assure compatibility with anticipated loads, provide unambiguous instruction for design and installation of cooling equipment, prevent oversizing, maximize electrical efficiency, and be flexible enough to work in various shapes and types of closets. This paper describes the science and practical application of an improved method for the specification of cooling for wiring closets.
WP-72 v1
Five Basic Steps for Efficient Space Organization within High Density Enclosures Organizing components and cables within high density enclosures need not be a stressful, time consuming chore. In fact, thanks to the flexibility of new enclosure designs, a standard for organizing enclosure space, including power and data cables can be easily implemented. This paper provides a five step roadmap for standardizing and optimizing organization within both low and high density enclosures, with special emphasis on how to plan for higher densities.
WP-50 v1
Cooling Solutions for Rack Equipment with Side-to-Side Airflow Equipment with side-to-side airflow presents special cooling challenges in the modern data center. Common rack enclosures and rack layouts are fundamentally incompatible with side-to-side cooling, resulting in equipment that receives supply air of excessive temperature. This paper describes the problem along with several side-effects that are not generally appreciated. Various solutions to the problem are described along with their costs and benefits.
Instructions for linking white paper content to your site
Since these white papers are often revised, to ensure your readers are receiving the most up-to-date content, it is important to use the following URL format when linking to these white papers:
http://www.apc.com/whitepaper/?wp=xxx
where "xxx" should be replaced with the number of the white paper being linked to.
Alternatively, the entire Schneider Electric data center white paper library can be linked to using the following url:
http://whitepapers.apc.com