ATTENTION: For instructions on how to properly link to these white papers.click here
4 result(s) found.
Number
Title & Abstract
WP-1 v7
The different types of UPS systems There is much confusion in the marketplace about the different types of UPS systems and their characteristics. Each of these UPS types is defined, practical applications of each are discussed, and advantages and disadvantages are listed. With this information, an educated decision can be made as to the appropriate UPS topology for a given need.
WP-8 v2
Inter-system Ground Noise: Causes and Effects Many power-related problems are the result of Inter-System Ground Noise. This problem cannot be corrected using typical AC-only power protection equipment. The cause and solution of Inter-System Ground Noise problems are described.
WP-10 v3
Preventing Data Corruption in the Event of an Extended Power Outage Despite advances in computer technology, power outages continue to be a major cause of PC and server downtime. Protecting computer systems with Uninterruptible Power Supply (UPS) hardware is part of a total solution, but power management software is also necessary to prevent data corruption after extended power outages. Various software configurations are discussed, and best practices aimed at ensuring uptime are presented.
Instructions for linking white paper content to your site
Since these white papers are often revised, to ensure your readers are receiving the most up-to-date content, it is important to use the following URL format when linking to these white papers:
http://www.apc.com/whitepaper/?wp=xxx
where "xxx" should be replaced with the number of the white paper being linked to.
Alternatively, the entire Schneider Electric data center white paper library can be linked to using the following url:
http://whitepapers.apc.com