White Papers

Search
Keyword:
-or-
Application:
-or-
Number:

133 result(s) found.
Number Abstract Type Size
WP-150 v2 Power and Cooling Capacity Management for Data Centers
High density IT equipment stresses the power density capability of modern data centers. Installation and unmanaged proliferation of this equipment can lead to unexpected problems with power and cooling infrastructure including overheating, overloads, and loss of redundancy. The ability to measure and predict power and cooling capability at the rack enclosure level is required to ensure predictable performance and optimize use of the physical infrastructure resource. This paper describes the principles for achieving power and cooling capacity management.
2140 KB
WP-0 v0 WHITE PAPER LIBRARY NAVIGATION GUIDE
This presentation provides recommended white paper reading lists by interest area, from fundamentals to best practices to hot topics.
144 KB
WP-118 v3 Virtualization and Cloud Computing: Optimized Power, Cooling, and Management Maximizes Benefits
IT virtualization, the engine behind cloud computing, can have significant consequences on the data center physical infrastructure (DCPI). Higher power densities that often result can challenge the cooling capabilities of an existing system. Reduced overall energy consumption that typically results from physical server consolidation may actually worsen the data center’s power usage effectiveness (PUE). Dynamic loads that vary in time and location may heighten the risk of downtime if rack-level power and cooling health are not understood and considered. Finally, the fault-tolerant nature of a highly virtualized environment could raise questions about the level of redundancy required in the physical infrastructure. These particular effects of virtualization are discussed and possible solutions or methods for dealing with them are offered.
1528 KB
WP-135 v2 Impact of Hot and Cold Aisle Containment on Data Center Temperature and Efficiency
Both hot-air and cold-air containment can improve the predictability and efficiency of traditional data center cooling systems. While both approaches minimize the mixing of hot and cold air, there are practical differences in implementation and operation that have significant consequences on work environment conditions, PUE, and economizer mode hours. The choice of hot-aisle containment over cold-aisle containment can save 43% in annual cooling system energy cost, corresponding to a 15% reduction in annualized PUE. This paper examines both methodologies and highlights the reasons why hot-aisle containment emerges as the preferred best practice for new data centers.
686 KB
WP-134 v2 Deploying High-Density Pods in a Low-Density Data Center
Simple and rapid deployment of self-contained, high-density pods within an existing or new low-density data center is possible with today’s power and cooling technology. The independence of these high-density pods allow for predictable and reliable operation of high-density equipment without a negative impact on the performance of existing low-density power and cooling infrastructure. A side benefit is that these high-density pods operate at much higher electrical efficiency than conventional designs. Guidance on planning design, implementation, and predictable operation of high-density pods is provided.
3636 KB
WP-163 v1 Containerized Power and Cooling Modules for Data Centers
Standardized, pre-assembled and integrated data center facility power and cooling modules are at least 60% faster to deploy, and provide a first cost savings of 13% or more compared to traditional data center power and cooling infrastructure. Facility modules, also referred to in the data center industry as containerized power and cooling plants, allow data center designers to shift their thinking from a customized "construction" mentality to a standardized "site integration" mentality. This white paper compares the cost of both scenarios, presents the advantages and disadvantages of each, and identifies which environments can best leverage the facility module approach.
1946 KB
WP-104 v2 Classification of Data Center Management Software Tools
Data centers today lack a formal system for classifying software management tools. As a result, confusion exists regarding which management systems are necessary and which are optional for secure and efficient data center operation. This paper divides the realm of data center management tools into four distinct subsets and compares the primary and secondary functions of key subsystems within these subsets. With a classification system in place, data center professionals can begin to determine which physical infrastructure management tools they need – and don’t need – to operate their data centers.
1845 KB
WP-107 v1 How Data Center Infrastructure Management Software Improves Planning and Cuts Operational Costs
Business executives are challenging their IT staffs to convert data centers from cost centers into producers of business value. Data centers can make a significant impact to the bottom line by enabling the business to respond more quickly to market demands. This paper demonstrates, through a series of examples, how data center infrastructure management software tools can simplify operational processes, cut costs, and speed up information delivery.
1004 KB
WP-132 v0 Economizer Modes of Data Center Cooling Systems
In certain climates, some cooling systems can save over 70% in annual cooling energy costs by operating in economizer mode, corresponding to over 15% reduction in annualized PUE. However, there are at least 17 different types of economizer modes with imprecise industry definitions making it difficult to compare, select, or specify them. This paper provides terminology and definitions for the various types of economizer modes and compares their performance against key data center attributes.
789 KB
WP-136 v0 High Efficiency Economizer-based Cooling Modules for Large Data Centers
When a cooling plant operates in economizer mode, high energy-consuming mechanical systems can be turned off. A standardized, modular cooling plant designed to operate primarily in economizer mode not only reduces costs but also improves predictability and flexibility. This paper shows a new approach to data center cooling that uses approximately half the energy of traditional methods, and at the same time provides greater scalability, availability, and ease of maintenance.
1295 KB
WP-126 v1 An Improved Architecture for High-Efficiency, High-Density Data Centers
Data center power and cooling infrastructure worldwide wastes more than 60, 000, 000 megawatt-hours per year of electricity that does no useful work powering IT equipment. This represents an enormous financial burden on industry, and is a significant public policy environmental issue. This paper describes the principles of a new, commercially available data center architecture that can be implemented today to dramatically improve the electrical efficiency of data centers.
1410 KB
WP-129 v1 A Scalable, Reconfigurable, and Efficient Data Center Power Distribution Architecture
Significant improvements in efficiency, power density, power monitoring, and reconfigurability have been achieved in data center power distribution. The past techniques of massive transformer-based power distribution units feeding under-floor hardwired circuits via rigid or flexible conduit are shown to be obsolete. This paper explains some the newer approaches to power distribution including modular power distribution and overhead power busway, and shows their advantages when compared to the legacy approach.
1242 KB
WP-114 v1 Implementing Energy Efficient Data Centers
Electricity usage costs have become an increasing fraction of the total cost of ownership (TCO) for data centers. It is possible to dramatically reduce the electrical consumption of typical data centers through appropriate design of the network-critical physical infrastructure and through the design of the IT architecture. This paper explains how to quantify the electricity savings and provides examples of methods that can greatly reduce electrical power consumption.
483 KB
WP-139 v0 Cooling Entire Data Centers Using Only Row Cooling
Row cooling is emerging as a practical total cooling solution for new data centers due to its inherent high efficiency and predictable performance. Yet some IT equipment in data centers appears incompatible with row cooling because it is not arranged in neat rows due to the nature of the equipment or room layout constraints, suggesting the ongoing need for traditional perimeter cooling to support these loads. This paper explains how a cooling system comprised only of row coolers, with no room cooling system, can cool an entire data center, including IT devices that are not in neat rows.
677 KB
WP-157 v0 Eco-mode: Benefits and Risks of Energy-saving Modes of UPS Operation
Many newer UPS systems have an energy-saving operating mode known as “eco-mode” or by some other descriptor. Nevertheless, surveys show that virtually no data centers actually use this mode, because of the known or anticipated side-effects. Unfortunately, the marketing materials for these operating modes do not adequately explain the cost / benefit tradeoffs. This paper shows that eco-mode typically provides a reduction of 2-4% in data center energy consumption and explains the various limitations and concerns that arise from eco-mode use. Situations where these operating modes are recommended and contra-indicated are also described.
418 KB
WP-175 v1 Preparing the Physical Infrastructure of Receiving Data Centers for Consolidation
The consolidation of one or more data centers into an existing data center is a common occurrence. This paper gives examples of what is becoming a standard architecture for preparing the physical infrastructure in the receiving data center. This approach allows for shorter timelines and high efficiency while avoiding the commonly expected difficulties and complexities often experienced with consolidation projects.
838 KB
WP-154 v2 Electrical Efficiency Measurement for Data Centers
Data center electrical efficiency is rarely planned or managed. The unfortunate result is that most data centers waste substantial amounts of electricity. Today it is both possible and prudent to plan, measure, and improve data center efficiency. In addition to reducing electrical consumption, efficiency improvements can gain users higher IT power densities and the ability to install more IT equipment in a given installation. This paper explains how data center efficiency can be measured, evaluated, and modeled, including a comparison of the benefits of periodic assessment vs. continuous monitoring.
1052 KB
WP-142 v1 Data Center Projects: System Planning
System planning is the Achilles’ heel of a data center physical infrastructure project. Planning mistakes can magnify and propagate through later deployment phases, resulting in delays, cost overruns, wasted time, and ultimately a compromised system. Much of the trouble can be eliminated by viewing system planning as a data flow model, with an orderly sequence of tasks that progressively transform and refine information from initial concept to final design.
4445 KB
WP-147 v0 Data Center Projects: Advantages of Using a Reference Design
It is no longer practical or cost-effective to completely engineer all aspects of a unique data center. Re-use of proven, documented subsystems or complete designs is a best practice for both new data centers and for upgrades to existing data centers. Adopting a well-conceived reference design can have a positive impact on both the project itself, as well as on the operation of the data center over its lifetime. Reference designs simplify and shorten the planning and implementation process and reduce downtime risks once up and running. In this paper reference designs are defined and their benefits are explained.
1481 KB
WP-158 v2 Guidance for Calculation of Efficiency (PUE) in Data Centers
Before data center infrastructure efficiency can be benchmarked using PUE or other metrics, there must be agreement on exactly what power consumptions constitute IT loads, what consumptions constitute physical infrastructure, and what loads should not be counted. Unfortunately, commonly published efficiency data is not computed using a standard methodology, and the same data center will have different efficiency ratings when different methodologies are applied. This paper explains the problem and describes a standardized method for classifying data center loads for efficiency calculations.
316 KB
WP-103 v0 How Monitoring Systems Reduce Human Error in Distributed Server Rooms and Remote Wiring Closets
Surprise incidences of downtime in server rooms and remote wiring closets lead to sleepless nights for many IT managers. Most can recount horror stories about how bad luck, human error, or just simple incompetence brought their server rooms down. This paper analyzes several of these incidents and makes recommendations for how a basic monitoring system can help reduce the occurrence of these unanticipated events.
930 KB
WP-42 v4 Ten Cooling Solutions to Support High-density Server Deployment
High-density servers offer a significant performance per watt benefit. However, depending on the deployment, they can present a significant cooling challenge. Vendors are now designing servers that can demand over 40 kW of cooling per rack. With most data centers designed to cool an average of no more than 2 kW per rack, innovative strategies must be used for proper cooling of high-density equipment. This paper provides ten approaches for increasing cooling efficiency, cooling capacity, and power density in existing data centers.
1130 KB
WP-161 v1 Allocating data center energy costs and carbon to IT users
Are complicated software and instrumentation needed to measure and allocate energy costs and carbon to IT users? Or can we get by with simple, low cost methods for energy cost and carbon allocation? How precise do we need to be? This paper provides an overview of energy cost and carbon allocation strategies and their precision. We show that it is both easy and inexpensive for any data center, large or small, new or old, to get started allocating costs and carbon, but the expense and complexity escalate and ROI declines when excessive precision is specified.
1179 KB
WP-177 v1 Determining the Power, Cooling, and Space Capacities when Consolidating Data Centers
When planning the consolidation of multiple data centers into existing data center(s), it is often difficult to establish the various capacities and capabilities of each site’s physical infrastructure. This information is a key input to deciding which site(s) will become the “receiving” data center(s). This paper describes how to specify these requirements in standard terms and how to establish current conditions and future capabilities of each data center involved in a consolidation project.
519 KB
WP-68 v1 Cooling Strategies for IT Wiring Closets and Small Rooms
Cooling for IT wiring closets is rarely planned and typically only implemented after failures or overheating occur. Historically, no clear standard exists for specifying sufficient cooling to achieve predictable behavior within wiring closets. An appropriate specification for cooling IT wiring closets should assure compatibility with anticipated loads, provide unambiguous instruction for design and installation of cooling equipment, prevent oversizing, maximize electrical efficiency, and be flexible enough to work in various shapes and types of closets. This paper describes the science and practical application of an improved method for the specification of cooling for wiring closets.
1211 KB
WP-122 v1 Guidelines for Specification of Data Center Criticality / Tier Levels
A framework for benchmarking a future data center’s operational performance is essential for effective planning and decision making. Currently available criticality or tier methods do not provide defensible specifications for validating data center performance. An appropriate specification for data center criticality should provide unambiguous defensible language for the design and installation of a data center. This paper analyzes and compares existing tier methods, describes how to choose a criticality level, and proposes a defensible data center criticality specification. Maintaining a data center’s criticality is also discussed.
1083 KB
WP-130 v1 The Advantages of Row and Rack-Oriented Cooling Architectures for Data Centers
Latest generation high density and variable density IT equipment create conditions that traditional data center room cooling was never intended to address, resulting in cooling systems that are inefficient, unpredictable, and low in power density. Row-oriented and rack-oriented cooling architectures have been developed to address these problems. This paper contrasts room, row, and rack architectures and shows why row-oriented cooling will emerge as the preferred solution for most next generation data centers.
758 KB
WP-7 v0 Maximizing Uptime in Mission-Critical Facilities
As technology reaches into every corner of our world, the importance of, and reliance on, your mission critical facility reaches new heights. Uptime is no longer a lofty goal, it is an absolute necessity. However, uptime is not a product that you specify with the design of your facility, install, and then forget about. A facility designed to 99.99% of availability will not achieve / maintain that number, unless we fully understand the many factors that affect uptime. Maximum Uptime is a philosophy. It begins with the planning of your facility, and remains a continuous process through every step of design, construction, commissioning, operations, failure analysis, and recommissioning.
119 KB
WP-28 v1 Rack Powering Options for High Density in 230VAC Countries
Alternatives for providing electrical power to high density racks in data centers and network rooms are explained and compared. Issues addressed include quantity of feeds, single-phase vs. three-phase, number and location of circuit breakers, overload, selection of connector types, selection of voltage, redundancy, and loss of redundancy. The need for the rack power system to adapt to changing requirements is identified and quantified. Guidelines are defined for rack power systems that can reliably deliver power to high density loads while adapting to changing needs.
702 KB
WP-159 v0 How Overhead Cabling Saves Energy in Data Centers
Placing data center power and data cables in overhead cable trays instead of under raised floors can result in an energy savings of 24%. Raised floors filled with cabling and other obstructions make it difficult to supply cold air to racks. The raised floor cable cutouts necessary to provide cable access to racks and PDUs result in a cold air leakage of 35%. The cable blockage and air leakage problems lead to the need for increased fan power, oversized cooling units, increased pump power, and lower cooling set points. This paper highlights these issues, and quantifies the energy impact.
802 KB
WP-120 v1 Guidelines for Specification of Data Center Power Density
Conventional methods for specifying data center density are ambiguous and misleading. Describing data center density using Watts / ft2 or Watts / m2 is not sufficient to determine power or cooling compatibility with high density computing loads like blade servers. Historically there is no clear standard way of specifying data centers to achieve predictable behavior with high density loads. An appropriate specification for data center density should assure compatibility with anticipated high density loads, provide unambiguous instruction for design and installation of power and cooling equipment, prevent oversizing, and maximize electrical efficiency. This paper describes the science and practical application of an improved method for the specification of power and cooling infrastructure for data centers.
473 KB
WP-160 v0 Specification of Modular Data Center Architecture
There is a growing consensus that conventional legacy data center design will be superseded by modular scalable data center designs. Reduced total cost of ownership, increased flexibility, reduced deployment time, and improved efficiency are all claimed benefits of modular scalable designs. Yet the term “modular”, when and where modularity is appropriate, and how to specify modularity are all poorly defined. This paper creates a framework for modular data center architecture and describes the various ways that modularity can be implemented for data center power, cooling, and space infrastructure and explains when the different approaches are appropriate and effective.
683 KB
WP-121 v1 Airflow Uniformity Through Perforated Tiles in a Raised-Floor Data Center
Perforated tiles on a raised floor often deliver substantially more or less airflow than expected, resulting in inefficiencies and even equipment failure due to inadequate cooling. In this paper, the impact of data center design parameters on perforated tile airflow is quantified and methods of improving airflow uniformity are discussed. This paper was written jointly by APC and IBM for the ASME InterPACK '05 conference.
1561 KB
WP-119 v1 Creating Order from Chaos in Data Centers and Server Rooms
Data center professionals can rid themselves of messy racks, sub-standard under floor air distribution, and cable sprawl with a minimum of heartache and expense. Whether the data center mess is created over years of mismanagement or whether the cable-choked data center is inherited, solutions for both quick fixes and longer term evolutionary changes exist. This paper outlines several innovative approaches for dealing with the symptoms of chaos and for eliminating the root causes of disorder.
1507 KB
WP-90 v1 Essential Standby Generator System Requirements for Next Generation Data Centers
Effective standby generator system installations must address the known problems and challenges relating to current and past designs. This paper presents a categorized and prioritized overview of generator system challenges and the requirements needed to overcome them.
359 KB
WP-127 v2 A Quantitative Comparison of High Efficiency AC vs. DC Power Distribution for Data Centers
This paper presents a detailed quantitative efficiency comparison between the most efficient DC and AC power distribution methods, including an analysis of the effects of power distribution efficiency on the cooling power requirement and on total electrical consumption. The latest high efficiency AC and DC power distribution architectures are shown to have virtually the same efficiency, suggesting that a move to a DC-based architecture is unwarranted on the basis of efficiency.
1093 KB
WP-55 v2 Air Distribution Architecture Options for Mission Critical Facilities
There are nine basic ways to use air to cool equipment in data centers and network rooms. These methods vary in performance, cost, and ease of implementation. These methods are described along with their various advantages. The proper application of these cooling techniques is essential knowledge for Information Systems personnel as well as Facilities Managers.
1429 KB
WP-49 v2 Avoidable Mistakes that Compromise Cooling Performance in Data Centers and Network Rooms
Avoidable mistakes that are routinely made when installing cooling systems and racks in data centers or network rooms compromise availability and increase costs. These unintentional flaws create hot-spots, decrease fault tolerance, decrease efficiency, and reduce cooling capacity. Although facilities operators are often held accountable for cooling problems, many problems are actually caused by improper deployment of IT equipment outside of their control. This paper examines these typical mistakes, explains their principles, quantifies their impacts, and describes simple remedies.
433 KB
WP-63 v6 AC vs DC Power Distribution for Data Centers
DC power distribution has been proposed as an alternative to AC power distribution in data centers, but misinformation and conflicting claims have confused the discussion. A detailed analysis and model show that many of the benefits commonly stated for DC distribution are unfounded or exaggerated. This paper explains why high efficiency AC will likely emerge as the dominant choice for data center power distribution.
318 KB
WP-46 v7 Cooling Strategies for Ultra-High Density Racks and Blade Servers
Rack power of 10 kW per rack or more can result from the deployment of high density information technology equipment such as blade servers. This creates difficult cooling challenges in a data center environment where the industry average rack power consumption is under 2 kW. Five strategies for deploying ultra-high power racks are described, covering practical solutions for both new and existing data centers.
763 KB
WP-116 v1 Standardization and Modularity in Data Center Physical Infrastructure
Failure to adopt modular standardization as a design strategy for data center physical infrastructure (DCPI) is costly on all fronts: unnecessary expense, avoidable downtime, and lost business opportunity. Standardization and its close relative, modularity, create wide-ranging benefits in DCPI that streamline and simplify every process from initial planning to daily operation, with significant positive effects on all three major components of DCPI business value – availability, agility, and total cost of ownership.
1794 KB
WP-58 v2 Humidification Strategies for Data Centers and Network Rooms
The control of humidity in Information Technology environments is essential to achieving high availability. This paper explains how humidity affects equipment and why humidity control is required. Quantitative design guidelines for existing and new computing installations are discussed. Alternative methods to achieve desired humidity are described and contrasted. The difficult issue of how and where humidity should be measured is explained. The hidden costs associated with over-humidification are described.
352 KB
WP-144 v1 Data Center Projects: Establishing a Floor Plan
A floor plan strongly affects the power density capability and electrical efficiency of a data center. Despite this critical role in data center design, many floor plans are established through incremental deployment without a central plan. Once a poor floor plan has been deployed, it is often difficult or impossible to recover the resulting loss of performance. This paper provides structured floor plan guidelines for defining room layouts and for establishing IT equipment layouts within existing rooms.
1276 KB
WP-102 v3 Monitoring Physical Threats in the Data Center
Traditional methodologies for monitoring the data center environment are no longer sufficient. With technologies such as blade servers driving up cooling demands and regulations such as Sarbanes-Oxley driving up data security requirements, the physical environment in the data center must be watched more closely. While well understood protocols exist for monitoring physical devices such as UPS systems, computer room air conditioners, and fire suppression systems, there is a class of distributed monitoring points that is often ignored. This paper describes this class of threats, suggests approaches to deploying monitoring devices, and provides best practices in leveraging the collected data to reduce downtime.
786 KB
WP-18 v1 The Seven Types of Power Problems
Many of the mysteries of equipment failure, downtime, software and data corruption, are often the result of a problematic supply of power. There is also a common problem with describing power problems in a standard way. This white paper will describe the most common types of power disturbances, what can cause them, what they can do to your critical equipment, and how to safeguard your equipment, using the IEEE standards for describing power quality problems.
535 KB
WP-140 v1 Data Center Projects: Standardized Process
As the design and deployment of data center physical infrastructure moves away from art and more toward science, the benefits of a standardized and predictable process are becoming compelling. Beyond the ordering, delivery, and installation of hardware, any build or upgrade project depends critically upon a well-defined process as insurance against surprises, cost overruns, delays, and frustration. This paper presents an overview of a standardized, step-by-step process methodology that can be adapted and configured to suit individual requirements.
898 KB
WP-145 v0 The Top 9 Mistakes in Data Center Planning
Why do so many data center builds and expansions fail? This white paper answers the question by revealing the top 9 mistakes organizations make when designing and building new data center space, and examines an effective way to achieve success through the Total Cost of Ownership (TCO) approach.
296 KB
WP-66 v0 Estimating a Data Center’s Electrical Carbon Footprint
Data center carbon emissions are a growing global concern. The U.S. Environmental Protection Agency (EPA) cites data centers as a major source of energy consumption in the United States. The EPA has set an efficiency target for government data centers: a 20% reduction in carbon footprint by 2011. European Union (EU) members have agreed to cut their combined emissions of greenhouse gases to 8% below the 1990 level by 2012. Data center owners will be increasingly challenged to report their carbon emissions. This paper introduces a simple approach, supported by free web-based tools, for estimating the carbon footprint of a data center anywhere in the world.
1071 KB
WP-27 v3 Efficiency and Other Benefits of 208 Volt Over 120 Volt Input for IT Equipment
Decisions made regarding the distribution of 208V or 120V power to IT equipment can significantly impact overall efficiency of the data center. This paper explores the voltage connection options of 208 volt (V) and 120V for servers in North America and considers the efficiency implications of these choices. This same discussion applies to the use of 200V vs. 100V in Japan.
175 KB
WP-141 v1 Data Center Projects: Project Management
In data center design/build projects, flaws in project management and coordination are a common – but unnecessary – cause of delays, expense, and frustration. The ideal is for project management activities to be structured and standardized like interlocking building blocks, so all parties can communicate with a common language, avoid responsibility gaps and duplication of effort, and achieve an efficient process with a predictable outcome. This paper presents a framework for project management roles and relationships that is understandable, comprehensive, and adaptable to any size project.
786 KB
WP-124 v1 Preventive Maintenance Strategy for Data Centers
In the broadening data center cost-saving and energy efficiency discussion, data center physical infrastructure preventive maintenance (PM) is sometimes neglected as an important tool for controlling TCO and downtime. PM is performed specifically to prevent faults from occurring. IT and facilities managers can improve systems uptime through a better understanding of PM best practices. This white paper describes the types of PM services that can help safeguard the uptime of data centers and IT equipment rooms. Various PM methodologies and approaches are discussed. Recommended practices are suggested.
845 KB
WP-48 v1 Comparing Availability of Various Rack Power Redundancy Configurations
Transfer switches and dual-path power distribution to IT equipment are used to enhance the availability of computing systems. Statistical availability analysis techniques suggest large differences in availability are expected between the various methods commonly employed. This paper examines various electrical architectures for redundancy that are implemented in today’s mission-critical environments. The availability analyses of these various scenarios are then performed and the results are presented. The analysis identifies which approach provides the best overall performance, and how alternatives compare in performance and value.
478 KB
WP-5 v0 A Practical Guide to Disaster Avoidance in Mission-Critical Facilities
A disaster preparedness plan is crucial to organizations operating in 24/7/365 environments. With zero disruption the goal, management must carefully evaluate and mitigate risks to the physical infrastructure that supports the mission-critical facility. While business continuity planning typically addresses Information Technology, this paper reviews and discusses the requirements of the facility’s infrastructure as part of a comprehensive business continuity disaster plan. Without a proper disaster mitigation plan for the facility’s infrastructure, the overall business continuity plan is built on a risky foundation. If a natural, human, or technological disaster strikes your facility, are you and your infrastructure prepared? Does your organization have procedures in place to prepare for severe winter storms, earthquakes, tornados, hurricanes, or other disasters? Surviving tomorrow’s disaster requires planning today.
142 KB
WP-108 v3 Making Large UPS Systems More Efficient
As energy resources become scarcer and more expensive, electrical efficiency is becoming a more important performance factor in the specification and selection of large UPS systems. There are three subtle but significant factors that can materially affect a company’s cost of operating a UPS system and particularly the electrical bill. Unfortunately, the people who specify systems often fail to recognize these factors, which leads to increased costs to the owner because operational efficiencies are not correctly considered. This paper discusses the common errors and misunderstandings in evaluating UPS efficiency. UPS efficiency curves are explained, compared, and their cost implications quantified.
600 KB
WP-40 v3 Cooling Audit for Identifying Potential Cooling Problems in Data Centers
The compaction of Information Technology equipment and simultaneous increases in processor power consumption are creating challenges for data center managers in ensuring adequate distribution of cool air, removal of hot air and sufficient cooling capacity. This paper provides a checklist for assessing potential problems that can adversely affect the cooling environment within a data center.
1190 KB
WP-125 v2 Strategies for Deploying Blade Servers in Existing Data Centers
When blade servers are densely packed, they can exceed the power and cooling capacities of almost all traditional data centers. This paper explains how to evaluate the options and select the best power and cooling approach for a successful and predictable blade deployment.
1156 KB
WP-98 v0 The Role of Isolation Transformers in Data Center UPS Systems
Most modern UPS systems do not include the internal transformers that were present in earlier designs. This evolution has increased efficiency while decreasing the weight, size, and raw materials consumption of UPS systems. In the new transformerless UPS designs, the transformers are optional and can be placed in the best location to achieve a required purpose. In older designs, transformers were typically installed in permanent positions where they provided no benefit, reduced system efficiency, or were not optimally located. This paper considers the function of transformers in UPS systems, when and how transformers should be used, and how the absence of internal transformers in newer UPS designs frequently improves data center design and performance.
559 KB
WP-29 v6 Rack Powering Options for High Density
Alternatives for providing electrical power to high density racks in Data Centers and Network Rooms are explained and compared. Issues addressed include quantity of feeds, single-phase vs. three-phase, number and location of circuit breakers, overload, selection of plug types, selection of voltage, redundancy, and loss of redundancy. The need for the rack power system to adapt to changing requirements is identified and quantified. Guidelines are defined for rack power systems that can reliably deliver power to high density loads while adapting to changing needs.
823 KB
WP-143 v1 Data Center Projects: Growth Model
Long term data center or network room capacity planning may seem impossible in the face of evolving IT technology and business requirements. Nevertheless, data center facilities have a lifetime that may span many generations of IT equipment, so planning – or lack of planning – can have a large impact on the effectiveness of investments. Many unnecessary costs can be avoided with simple planning strategies, and even uncertainty itself can be incorporated into a plan. This paper shows a simple and effective way to develop a capacity plan for a data center or network room.
1689 KB
WP-131 v1 Improved Chilled Water Piping Distribution Methodology for Data Centers
Chilled water remains a popular cooling medium; however leaks in the piping systems are a threat to system availability. High density computing creates the need to bring chilled water closer than ever before to the IT equipment, prompting the need for new high reliability piping methods. This paper discusses new piping approaches which can dramatically reduce the risk of leakage and facilitate high density deployment. Alternative piping approaches and the advantages over traditional piping systems are described.
883 KB
WP-176 v1 Energy Savings Performance Contracts for Federal Data Center Consolidation
The cost of operating and maintaining federal agency data centers is extremely high. Mandates and initiatives have been put in place to address these costs through energy conservation, but with budgets already strained, the initial capital investment can be a daunting hurdle. This paper describes energy savings performance contracts (ESPCs), explains how to use them as an alternative financing option for consolidation projects, and provides examples.
241 KB
WP-128 v2 High-Efficiency AC Power Distribution for Green Data Centers
The use of 240 volt power distribution for data centers saves floor space, simplifies power cabling, saves capital cost, reduces weight, and increases electrical efficiency. This paper describes the various con-figurations for this distribution architecture and quantifies the benefits for the optimal configuration. Note: The methods in this paper only apply in North America and are for problems that are unique to North America.
531 KB
WP-6 v4 Determining Total Cost of Ownership for Data Center and Network Room Infrastructure
An improved method for measuring total cost of ownership (TCO) of data center and network room physical infrastructure and relating these costs to the overall Information Technology infrastructure is described, with examples. The cost drivers of TCO are quantified. The largest cost driver is shown to be unnecessary unabsorbed costs resulting from the oversizing of the infrastructure.
232 KB
WP-92 v2 Comparison of Static and Rotary UPS
Much confusion exists among data center professionals when deciding whether to deploy static or rotary Uninterruptible Power Supplies (UPS) in their data centers. This paper defines both static and rotary UPS architectures, points out similarities and differences, and analyzes the advantages and disadvantages of each in data center environments.
1134 KB
WP-137 v1 Energy Efficient Cooling for Data Centers: A Close-Coupled Row Solution
The trend of increasing heat densities in data centers has held consistent with advances in computing technology for many years. As power density increased, it became evident that the degree of difficulty in cooling these higher power loads was also increasing. In recent years, traditional cooling system design has proven inadequate to remove concentrated heat loads (20 kW per rack and higher). This has driven an architectural shift in data center cooling. The advent of a newer cooling architecture designed for these higher densities has brought with it increased efficiencies for the data center. This article discusses the efficiency benefits of row-based cooling compared to two other common cooling architectures.
1868 KB
WP-44 v4 Improving Rack Cooling Performance Using Airflow Management Blanking Panels
Unused vertical space in open frame racks and rack enclosures creates an unrestricted recycling of hot air that causes equipment to heat up unnecessarily. The use of airflow management blanking panels can reduce this problem. This paper explains and quantifies the effects of airflow management blanking panels on cooling system performance.
472 KB
WP-117 v1 Data Center Physical Infrastructure: Optimizing Business Value
To stay competitive in today’s rapidly changing business world, companies must update the way they view the value of their investment in data center physical infrastructure (DCPI). No longer are simply availability and upfront cost sufficient to make adequate business decisions. Agility, or business flexibility, and low total cost of ownership have become equally important to companies that will succeed in a changing global marketplace.
878 KB
WP-19 v2 Re-examining the Suitability of the Raised Floor for Data Center Applications
The circumstances that gave rise to the development and use of the raised floor in the data center environment are examined. Many of the reasons for the raised floor no longer exist, and the problems associated with raised floors suggest that their widespread use is no longer justified or desirable for many applications.
230 KB
WP-43 v3 Dynamic Power Variations in Data Centers and Network Rooms
The power requirement required by data centers and network rooms varies on a minute by minute basis depending on the computational load. This magnitude of this variation has grown and continues to grow dramatically with the deployment of power management technologies in servers and communication equipment. This variation gives rise to new problems relating to availability and management.
159 KB
WP-138 v1 Energy Impact of Increased Server Inlet Temperature
The quest for efficiency improvement raises questions regarding the optimal air temperature for data centers. The ASHRAE TC-9.9 committee has recently adopted an extension of the recommended thermal envelope for server inlet temperature and humidity. A popular hypothesis suggests that total energy demands should diminish as the server inlet temperatures increase. This paper tests that hypothesis through the development of a composite power consumption baseline for a mixture of servers as a function of inlet temperature and applying this data to a variety of cooling architectures.
488 KB
WP-73 v1 Reducing the Hidden Costs Associated with Upgrades of Data Center Power Capacity
Scaling the power capacity of legacy UPS systems leads to hidden costs that may outweigh the very benefit that scalability intends to provide. A scalable UPS system provides a significant benefit to the Total Cost of Ownership (TCO) of data center and network room physical infrastructure. This paper describes the drawbacks of scaling legacy UPS systems and how scalable rack-based systems address these drawbacks. The cost factors of both methods are described, quantified and compared.
279 KB
WP-109 v1 Reliability Analysis of the APC Symmetra MW Power System
This paper is a quantitaive reliability analysis of the APC Symmetra MW UPS performed by MTechnology, Inc. (MTech). In contrast to common MTBF calculations based on summing component failure rates, this study used techniques of Probabilistic Risk Assessment (PRA) to calculate the likelihood of over 680, 000 potential failure modes. The mathematical method accounts for uncertainty in failure rates and component performance, and provides detailed guidance as to the contribution of each system component to the overall risk of failure. The study included an exhaustive analysis of the system’s architecture, component selection, control system, manufacturing practices, and response to internal and external faults. The study also included a detailed review of APC’s delta conversion online topology.
307 KB
WP-250 v0 Guide for Reducing Data Center Physical Infrastructure Energy Consumption in Federal Data Centers
In an effort to create a clean energy economy, recent US presidents and congress have issued a series of legislation and executive orders requiring federal agencies to increase energy efficiency and reduce carbon emissions in government facilities. Vivek Kundra, Federal Chief Information Officer, is supporting that effort by establishing a Federal Data Center Consolidation Initiative to help reduce energy consumption in over 1, 100 Federal data centers. US Federal data center managers are on a timeline to respond with their final consolidation plan. This paper analyzes the implication of these mandates and offers recommendations for how to improve energy efficiency in Federal data centers. This paper is written for a US-only audience.
873 KB
WP-112 v1 Performing Effective MTBF Comparisons for Data Center Infrastructure
Mean Time Between Failure (MTBF) is often proposed as a key decision making criterion when comparing data center infrastructure systems. Misleading values are often provided by vendors, leaving the user incapable of making a meaningful comparison. When the variables and assumptions behind the numbers are unknown or are misinterpreted, bad decisions are inevitable. This paper explains how MTBF can be effectively used as one of several factors for specification and selection of systems, by making the assumptions explicit.
380 KB
WP-111 v1 Reliability Analysis of the APC InfraStruXure Power System
The APC InfraStruXure product line offers an alternative architecture to the central UPS. MTechnology, Inc. used the techniques of Probabilistic Risk Assessment (PRA) to evaluate the reliability of the 40 kW InfraStruXure UPS and PDU with static bypass. The calculations considered the performance of the InfraStruXure in both ideal and real-world conditions. The study also compared the performance of the InfraStruXure architecture to that of a central UPS serving a hypothetical 500 kW critical load in a data center. The results showed that the InfraStruXure architecture was significantly less likely to suffer failure of all loads in the data center, and slightly less likely to experience failure in any one piece of IT equipment. This paper summarizes the key findings of MTechnology's quantitative risk assessment and discusses their implications for facility managers and designers.
226 KB
WP-57 v4 Fundamental Principles of Air Conditioners for Information Technology
Every Information Technology professional who is responsible for the operation of computing equipment needs to understand the function of air conditioning in the data center or network room. This introductory paper explains the function of basic components of an air conditioning system for a computer room. The concepts presented here are a foundation for allowing IT professionals to successfully specify, install, and operate critical facilities.
357 KB
WP-65 v2 Comparing Data Center Batteries, Flywheels, and Ultracapacitors
Most data center professionals choose lead-acid batteries as their preferred method of energy storage. However, alternatives to lead-acid batteries are attracting more attention as raw material and energy costs continue to increase and as governments become more vigilant regarding environmental and waste disposal issues. This paper compares several popular classes of batteries, compares batteries to both flywheels and ultracapacitors, and briefly discusses fuel cells.
795 KB
WP-78 v1 Mean Time Between Failure: Explanation and Standards
Mean Time Between Failure is a reliability term used loosely throughout many industries and has become widely abused in some. Over the years the original meaning of this term has been altered which has led to confusion and cynicism. MTBF is largely based on assumptions and definition of failure and attention to these details are paramount to proper interpretation. This paper explains the underlying complexities and misconceptions of MTBF and the methods available for estimating it.
256 KB
WP-82 v2 Physical Security in Mission Critical Facilities
Physical security is critical to achieving availability goals of mission critical facilities. Security of the data center accounts for it’s surroundings as well as data processing equipment inside and the systems supporting them. In this paper, systems for providing secure facilities are recommended and best practices for physical security are explained.
511 KB
WP-52 v1 Four Steps to Determine When a Standby Generator is Needed for Small Data Centers
Small data centers and network rooms vary dramatically in regard to the amount of UPS runtime commonly deployed. This paper describes a rational framework for establishing backup time requirements. Tradeoffs between supplemental UPS batteries and standby generators are discussed, including a total cost of ownership (TCO) analysis to help identify which solution makes the most economic sense. The analysis illustrates that the runtime at which generators become more cost effective than batteries varies dramatically with kW and ranges from approximately 20 minutes to over 10 hours.
586 KB
WP-62 v1 Powering Single-Corded Equipment in a Dual Path Environment
The use of dual power path architecture in combination with IT equipment with dual power supplies and power cords is an industry best-practice. In facilities using this approach there are inevitably some IT devices which have only a single power cord. There are a number of options for integrating single-corded devices into a high availability dual path data center. This paper explains the differences between the various options and provides a guide to selecting the appropriate approach.
1039 KB
WP-1 v7 The different types of UPS systems
There is much confusion in the marketplace about the different types of UPS systems and their characteristics. Each of these UPS types is defined, practical applications of each are discussed, and advantages and disadvantages are listed. With this information, an educated decision can be made as to the appropriate UPS topology for a given need.
242 KB
WP-26 v1 Hazards of Harmonics and Neutral Overloads
This document provides an overview of problems related to harmonic currents, with a specific focus on Information Technology equipment. The way that international regulations solved these problems is described.
161 KB
WP-22 v4 Understanding EPO and its Downtime Risks
An Emergency Power Off (EPO) system is a control mechanism, formally known as a "disconnecting means." It is intended to power down a single piece of electronic equipment or an entire installation from a single point. EPO is employed in many applications such as industrial processes and information technology (IT). This white paper describes the advantages and disadvantages of EPO for protecting data centers and small IT equipment rooms containing uninterruptible power supply (UPS) systems. Various codes and standards that require EPO are discussed. Recommended practices are suggested for the use of EPO with UPS systems.
360 KB
WP-89 v1 Data Center Physical Infrastructure for Radio Frequency Identification (RFID) Systems
Radio frequency identification (RFID) technology helps automate a variety of business processes, improving their efficiencies. It generates a huge volume of data that needs to be filtered, processed and stored, and generally requires its own virtual local area network (VLAN). To gain all the promised benefits and return on investment of RFID, the network must be highly available. The data center physical infrastructure (DCPI) must be assessed for vulnerabilities in power, cooling, physical security, and other CCPI elements. Failing to plan for DCPI can lead to disruption of critical business processes resulting in loss of revenue and competitive advantage. This paper provides an understanding of an RFID network and its components, identifies critical DCPI locations, and explains how to plan for high availability.
771 KB
WP-88 v2 Power and Cooling Considerations for Power-over-Ethernet (PoE)
Power-over-Ethernet (PoE) can cut costs by enabling, for the first time, the deployment of a single Ethernet cable for simultaneous access to both power and data. However, lack of a power and cooling plan to support the PoE implementation can result in unanticipated downtime. This paper illustrates which power and cooling factors to consider when safeguarding a PoE investment.
1353 KB
WP-59 v1 The Different Types of Air Conditioning Equipment for IT Environments
Cooling equipment for an IT environment can be implemented in 10 basic configurations. The selection of the appropriate configuration for a particular installation is affected by the existing facility infrastructure, the total power level of the installation, the geographical location, and the physical constraints of the building. This document describes the 5 fundamental cooling transport methods that combine with 2 fundamental physical arrangements to give rise to the 10 basic configurations. A method for selection of the appropriate configuration for a particular installation is described. The information in this paper allows IT professionals to be more involved in the specification of precision cooling solutions that better align with IT objectives.
1495 KB
WP-69 v1 Power and Cooling for VoIP and IP Telephony Applications
Voice Over IP (VoIP) deployments can cause unexpected or unplanned power and cooling requirements in wiring closets and wiring rooms. Most wiring closets do not have uninterruptible power available, and they do not provide the ventilation or cooling required to prevent equipment overheating. Understanding the unique cooling and powering needs of VoIP equipment allows planning for a successful and cost effective VoIP deployment. This paper explains how to plan for VoIP power and cooling needs, and describes simple, fast, reliable, and cost effective strategies for upgrading old facilities and building new facilities.
907 KB
WP-8 v2 Inter-system Ground Noise: Causes and Effects
Many power-related problems are the result of Inter-System Ground Noise. This problem cannot be corrected using typical AC-only power protection equipment. The cause and solution of Inter-System Ground Noise problems are described.
285 KB
WP-37 v6 Avoiding Costs From Oversizing Data Center and Network Room Infrastructure
The physical and power infrastructure of data centers and network rooms is typically oversized by more than 100%. Statistics related to oversizing are presented. The costs associated with oversizing are quantified. The fundamental reasons why oversizing occurs are discussed. An architecture and method for avoiding oversizing is described.
255 KB
WP-56 v3 How and Why Mission-Critical Cooling Systems Differ From Common Air Conditioners
Today's technology rooms require precise, stable environments in order for sensitive electronics to operate optimally. Standard comfort air conditioning is ill suited for technology rooms, leading to system shutdowns and component failures. Because precision air conditioning maintains temperature and humidity within a very narrow range, it provides the environmental stability required by sensitive electronic equipment, allowing your business to avoid expensive downtime.
381 KB
WP-72 v1 Five Basic Steps for Efficient Space Organization within High Density Enclosures
Organizing components and cables within high density enclosures need not be a stressful, time consuming chore. In fact, thanks to the flexibility of new enclosure designs, a standard for organizing enclosure space, including power and data cables can be easily implemented. This paper provides a five step roadmap for standardizing and optimizing organization within both low and high density enclosures, with special emphasis on how to plan for higher densities.
2436 KB
WP-86 v1 Data Center Physical Infrastructure for Medical Imaging and Diagnostic Equipment
Medical imaging and diagnostic equipment (MIDE) is increasingly being networked to Picture Archiving and Communications Systems (PACS), Radiology Information Systems (RIS), Hospital Information Systems (HIS), and getting connected to the hospital intranet as well as the Internet. Failing to implement the necessary data center physical infrastructure (DCPI) can result in unexpected downtime, and safety and compliance issues, which translates into lost revenue and exposure to expensive litigations, negatively affecting the bottom line. This paper explains how to plan for DCPI when deploying medical imaging and diagnostic equipment, with emphasis on power and cooling.
858 KB
WP-50 v1 Cooling Solutions for Rack Equipment with Side-to-Side Airflow
Equipment with side-to-side airflow presents special cooling challenges in the modern data center. Common rack enclosures and rack layouts are fundamentally incompatible with side-to-side cooling, resulting in equipment that receives supply air of excessive temperature. This paper describes the problem along with several side-effects that are not generally appreciated. Various solutions to the problem are described along with their costs and benefits.
1062 KB
WP-38 v1 Harmonic Currents in the Data Center: A Case Study
This document provides an overview of how problems related to harmonic neutral currents are mitigated by load diversity, with specific focus on Information Technology data center environments. Detailed measurements of an actual operating data center are presented. This case study illustrates the way that load diversity mitigates harmonic current levels, lowers shared neutral current in multi-wire feeders and branch circuits, and improves total circuit power factor.
231 KB
WP-36 v1 Data Center VRLA Battery End-of-Life Recycling Procedures
Contrary to popular belief, the recycling of lead-acid batteries, which are the most common batteries found in data centers, is one of the most successful recycling systems that the world has ever seen. Reputable battery manufacturers, suppliers, and recycling companies have teamed up to establish a mature and highly efficient lead-acid battery recycling process. This paper reviews battery end-of-life options and describes how a reputable vendor can greatly facilitate the safe disposal and recycling of VRLA lead-acid batteries.
753 KB
WP-148 v1 Data Center Projects: Commissioning
Failure to properly commission a data center leaves the door wide open for expensive and disruptive downtime that could have been avoided. Integrated commissioning of all physical infrastructure components assures maximum data center performance and justifies the physical infrastructure investment. This paper reviews the desired outputs and identifies the standard inputs of the commissioning data center project step. The commissioning process flow is described and critical success factors are discussed. The commissioning process inputs and outputs are also placed in context with other key data center project process phases and steps.
997 KB
WP-15 v1 Watts and Volt-Amps: Powerful Confusion
This note helps explain the differences between Watts and VA and explains how the terms are correctly and incorrectly used in specifying power protection equipment.
150 KB
WP-149 v1 Ten Errors to Avoid When Commissioning a Data Center
Data center commissioning can deliver an unbiased evaluation of whether a newly constructed data center will be an operational success or a failure. Proper execution of the commissioning process is a critical step in determining how the data center operates as an integrated system. The documentation produced as a result of commissioning is also the single, most enduring value added deliverable in a data center’s operational life. This paper outlines the ten most common errors that prevent successful execution of the commissioning process.
185 KB
WP-84 v1 Data Center Physical Infrastructure for Enterprise Wireless LANs
Wireless LAN (WLAN) deployments can result in unexpected or unplanned power, cooling, management and security requirements. Most wiring closets do not have uninterruptible power supplies (UPS), and they do not provide adequate ventilation or cooling required to prevent equipment overheating. Understanding the unique data center physical infrastructure (DCPI) requirements of WLAN equipment allows planning for a successful and cost effective deployment. This paper explains how to plan for DCPI while deploying indoor WLANs in small, medium or large enterprise, with emphasis on power and cooling. Simple, fast, reliable, and cost effective strategies for upgrading old facilities or building new facilities are described.
1253 KB
WP-24 v3 Effect of UPS on System Availability
This white paper explains how system availability and uptime are affected by AC power outages and provides quantitative data regarding uptime in real-world environments, including the effect of UPS on uptime.
159 KB
WP-11 v3 Explanation of Cooling and Air Conditioning Terminology for IT Professionals
As power densities continue to increase in today’s data centers, heat removal is becoming a greater concern for the IT professional. Unfortunately, air conditioning terminology routinely used in the cooling industry is unnecessarily complicated. This complexity makes it difficult and frustrating for IT professionals to specify cooling requirements and even makes it difficult to discuss current cooling system performance with contractors, engineers, and maintenance personnel. This paper explains cooling terms in common language, providing an essential reference for IT professionals and data center operators.
259 KB
WP-25 v3 Calculating Total Cooling Requirements for Data Centers
This document describes how to estimate heat output from Information Technology equipment and other devices in a data center such as UPS, for purposes of sizing air conditioning systems. A number of common conversion factors and design guideline values are also included.
206 KB
WP-79 v1 Technical comparison of On-line vs. Line-interactive UPS designs
UPS systems below 5000VA are available in two basic designs: line-interactive or double-conversion on-line. This paper describes the advantages and disadvantages of each topology and addresses some common misconceptions about real-world application requirements.
268 KB
WP-115 v1 Accounting and Tax Benefits of Modular, Portable Data Center Infrastructure
Well-informed accounting treatment of data center physical infrastructure (DCPI) assets provides significant opportunities to contribute to improving the financial performance of a business, institution, or organization. Design and manufacturing improvements in modular, scalable UPS systems, power distribution units (PDUs), and computer room air conditioners have not only created technological benefits, but provide entirely new DCPI asset management opportunities with direct and measurable financial benefits.
246 KB
WP-3 v1 Calculating Total Power Requirements for Data Centers
Part of data center planning and design is to align the power and cooling requirements of the IT equipment with the capacity of infrastructure equipment to provide it. This paper presents methods for calculating power and cooling requirements and provides guidelines for determining the total electrical power capacity needed to support the data center, including IT equipment, cooling equipment, lighting, and power backup.
220 KB
WP-87 v1 Use of the Signal Reference Grid in Data Centers
Signal reference grids are automatically specified and installed in data centers despite the fact that they are no longer needed by modern IT equipment. Even when installed, they are typically used incorrectly. This paper explains the origins of the signal reference grid, the operating principles and limitations, and why they no longer are needed.
267 KB
WP-96 v1 A Hidden Reliability Threat in UPS Static Bypass Switches
IT managers will be surprised to learn that some medium and high power UPS systems on the market today (rated 50 kW and higher) use undersized static bypass switches despite their negative implications. By using a contactor or a circuit breaker in parallel with SCRs, these static bypass switches are able use smaller, less expensive SCRs that are rated to carry less than full load current continuously. This paper shows that the availability of the UPS system is compromised when undersized static bypass switches are employed in the system. The advantages of fully rated static bypass switches are discussed.
172 KB
WP-64 v2 Alternative Power Generation Technologies for Data Centers and Network Rooms
Fuel Cells and Micro Turbines are new technology alternatives for power generation for data centers and network rooms. This paper discusses the various modes of operation of these systems and examines benefits and drawbacks of the technologies when contrasted with conventional alternatives such as standby generators.
218 KB
WP-34 v2 Battery Technology for Data Centers and Network Rooms: Ventilation
Lead-acid batteries are the most widely used method of energy reserve. Ventilation systems must address health and safety as well as performance of the battery and other equipment in a room. Valve Regulated Lead Acid (VRLA) batteries and modular battery cartridges (MBC) do not require special battery rooms and are suitable for use in an office environment. Air changes designed for human occupancy normally exceed the requirements for VRLA and MBC ventilation. Vented (flooded) batteries, which release hydrogen gas continuously, require a dedicated battery room with ventilation separate from the rest of the building. This paper summarizes some of the factors and codes to consider when selecting and sizing a ventilation system for a facility in which stationary batteries are installed.
250 KB
WP-85 v1 Data Line Transient Protection
Electrical transients (surges) on data lines can destroy computing equipment both in the business and home office environments. Many users appreciate the risk of power surges but overlook data line surges. This white paper explains how transients are created, how they can have devastating effects on electrical equipment, and how surge suppression devices work to help protect against them.
218 KB
WP-35 v3 Battery Technology for Data Centers and Network Rooms: Lifecycle Costs
The lifecycle cost of different UPS battery technologies is compared. The costs associated with the purchase of batteries, the infrastructure costs, and the costs associated with inflexibility to meet changing requirements are discussed and quantified.
212 KB
WP-81 v1 Site Selection for Mission Critical Facilities
When selecting a new site or evaluating an existing site, there are dozens of risk factors that must be considered if optimal availability is to be obtained. Geographic, site-related, building, and economic risks need to be understood and mitigated to lessen the downtime effects on your business. In this paper guidelines are established for selecting a new site or assessing an existing one. Common risks that affect the availability of a business are defined and techniques for minimizing these risks are presented.
1972 KB
WP-60 v1 Avoiding AC Capacitor Failures in Large UPS Systems
Most AC power capacitor failures experienced in large UPS systems are avoidable. Capacitor failures can give rise to UPS failure and can in some cases cause critical load drops on stand-alone and paralleled systems. AC capacitor failures have historically been ascribed to unavoidable random failure or supplier defect. However, recent advances in the science of capacitor reliability analysis show that capacitor failures can be controlled by system design. This paper explains AC capacitor failure mechanisms and demonstrates how UPS designers and specifiers can avoid most common AC capacitor failures and the associated consequences.
455 KB
WP-30 v12 Battery Technology for Data Centers and Network Rooms: Lead-Acid Battery Options
The lead-acid battery is the predominant choice for Uninterruptible Power Supply (UPS) energy storage. Over 10 million UPSs are presently installed utilizing Flooded, Valve Regulated Lead Acid (VRLA), and High Density Modular Battery Cartridges (HDBCMBC) systems. This paper discusses the advantages and disadvantages of these three battery technologies.
359 KB
WP-17 v1 Understanding Power Factor, Crest Factor, and Surge Factor
This white paper explains the technical terms of power factor, crest factor, and surge factor. The use of these terms in specifying UPS is explained.
155 KB
WP-20 v1 The Different Types of AC Power Connectors in North America
A confusing array of AC power plugs and receptacles exist to deliver power to various electronic loads. This white paper describes the different types of connectors used to power computer equipment in North America. An illustration guide is provided in the appendix to help identify the various connectors by appearance and size.
243 KB
WP-33 v4 Battery Technology for Data Centers and Network Rooms: Site Planning
The choice of UPS battery technology directly impacts site requirements and the costs for protecting information technology and network environments. This paper will discuss how battery technologies impact site requirements.
186 KB
WP-39 v2 Battery Technology for Data Centers and Network Rooms: VRLA Reliability and Safety
The Valve Regulated lead-Acid (VRLA) battery is the predominant choice for small and medium-sized Uninterruptible Power Supply (UPS) energy storage. This white paper explores how the technology affects overall battery life and system reliability. It will examine the expected performance, life cycle factors, and failure mechanisms of VRLA batteries.
491 KB
WP-76 v1 Modular Systems: The Evolution of Reliability
Nature proved early on that in complex systems, modular designs are the ones that survive and thrive. An important contributor to this success is the critical reliability advantage of fault tolerance, in which a modular system can shift operation from failed modules to healthy ones while repairs are made. In data centers, modular design has already taken root in new fault-tolerant architectures for servers and storage systems. As data centers continue to evolve and borrow from nature’s blueprints, data center physical infrastructure (DCPI) must also evolve to support new strategies for survival, recovery, and growth.
525 KB
WP-31 v7 Battery Technology for Data Centers and Network Rooms: Fire Safety Codes - USA
Fire safety regulations and their application to UPS battery installations are reviewed. In some cases, fire codes do not clearly recognize improvements in battery safety resulting from changing battery technology. Valve Regulated Lead Acid (VRLA) batteries are frequently deployed within data centers and network rooms without the need for the elaborate safety systems that are required for Vented (Flooded) Lead Acid batteries. Proper interpretation of the fire codes is essential in the design and implementation of data centers and network rooms.
190 KB
WP-32 v7 Battery Technology for Data Centers and Network Rooms: Environmental Regulations
Some lead-acid batteries located in data centers are subject to government environmental compliance regulations. While most commercial battery back-up systems fall below required reporting levels, very large UPS and DC plant batteries may have to comply. Failure to comply can result in costly penalties. Environmental compliance regulations focus on the amount of sulfuric acid and lead in a given location. This paper offers a high level summary of the regulations and provides a list of environmental compliance information resources.
319 KB
WP-75 v3 Comparing UPS System Design Configurations
There are five principle UPS system design configurations that distribute power from the utility source of a building to the critical loads of a data center. The selection of the appropriate configuration or combination thereof for a particular application is determined by the availability needs, risk tolerance, types of loads in the data center, budgets, and existing infrastructure. This paper will focus on these five configurations; the advantages and disadvantages of each are discussed. The impact on availability is addressed for each configuration and guidelines are provided for choosing the appropriate design.
518 KB
WP-10 v3 Preventing Data Corruption in the Event of an Extended Power Outage
Despite advances in computer technology, power outages continue to be a major cause of PC and server downtime. Protecting computer systems with Uninterruptible Power Supply (UPS) hardware is part of a total solution, but power management software is also necessary to prevent data corruption after extended power outages. Various software configurations are discussed, and best practices aimed at ensuring uptime are presented.
445 KB
WP-9 v2 Common Mode Susceptibility of Computers
This white paper examines and challenges the claims made in literature regarding the alleged high susceptibility of computers to common mode noise.
583 KB
WP-101 v1 Fundamental Principles of Network Security
Security incidents are rising at an alarming rate every year. As the complexity of the threats increases, so do the security measures required to protect networks. Data center operators, network administrators, and other data center professionals need to comprehend the basics of security in order to safely deploy and manage networks today. This paper covers the fundamentals of secure networking systems, including firewalls, network topology and secure protocols. Best practices are also given that introduce the reader to some of the more critical aspects of securing a network.
663 KB
WP-21 v1 Neutral Wire Facts and Mythology
This Technical Note discusses many common misunderstandings about the function of the neutral wire and its relation to power problems. The subjects of dedicated lines, phase reversal, isolation transformers, and grounding are addressed. Various myths are described and criticized.
199 KB
WP-123 v1 Impact of High Density Hot Aisles on IT Personnel Work Conditions
The use of modern enclosed hot aisles to address increasing power densities in the data center has brought into question the suitability of working conditions in these hot aisle environments. In this paper, it is determined that the additional heat stress imposed by such high density IT environments is of minimal concern.
634 KB
WP-93 v1 Fundamental Principles of Generators for Information Technology
Every Information Technology professional who is responsible for the operation of computing equipment needs to ensure their data center or network room is prepared for extended utility power outages. Understanding the basic functions and concepts of standby generator systems helps provide a solid foundation allowing IT professionals to successfully specify, install, and operate critical facilities. This paper is an introduction to standby generators and subsystems that power a facility’s critical electrical loads when the utility cannot.
560 KB
WP-113 v2 Electrical Efficiency Modeling for Data Centers
Conventional models for estimating electrical efficiency of data centers are grossly inaccurate for real-world installations. Estimates of electrical losses are typically made by summing the inefficiencies of various electrical devices, such as power and cooling equipment. This paper shows that the values commonly used for estimating equipment inefficiency are quite inaccurate. A simple, more accurate efficiency model is described that provides a rational basis to identify and quantify waste in power and cooling equipment.
1066 KB
WP-83 v2 Mitigating Fire Risks in Mission Critical Facilities
This paper provides a clear understanding of the creation, detection, suppression, and prevention of fire within mission critical facilities. Fire codes for Information Technology environments are discussed. Best practices for increasing availability are provided.
436 KB
WP-16 v1 Protection of RS-232 Serial Connections
This white paper explains the special power protection issues related to RS-232 cabling. First, the special vulnerabilities of RS-232 cabling are explained. Then appropriate protection and mitigation techniques are provided.
185 KB
WP-23 v1 Reliability Models for Electric Power Systems
This white paper explains the sources of downtime in electric power systems and provides an explanation for site-to-site variations in power availability. The factors affecting power quality from generation to the utilization point are summarized. There is a qualitative description of a model, which can be combined with data to provide a method for estimating down time based on site-related factors.
158 KB