FAQ

:
-or-
:

1 result(s) found.
Title Type Size
FAQ on the Upgrade of SYPM10KH to SYPM10K16H
The SYPM10K16H power module was developed as part of the second generation symmetra PX, 400V product line. It was made backward compatible with the existing SYPM10KH, 400V module to allow it to be used as its replacement. This FAQ answers many of the common questions we received regarding the transition of the SYPM10KH to the new SYPM10K16H module.
66 KB